2389681_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2389681_en-US

2389681_en-US

LS1043AXN8QQB DVFS

Dear support,

 The customer used the LS1043AXN8QQB platform and set the CPU dynamic frequency adjustment from 1.6GHz to 800MHz and 500MHz. It was found that RCU stall and PCIE communication abnormality occurred when the CPU ran at 500MHz.

According to the RM and datasheet of the chip, LS1043 supports 1GHz to 1.6GHz. The official document does not mention the minimum supported frequency for dynamic frequency adjustment. It is uncertain whether 500MHz is supported?

Does LS1043A support dynamic frequency adjustment when the CPU is running normally?

the customer projects (LS1043AXN8QQB ) used version:

Linux 5.4.301

LS1043A RDB Board

4-cores CPU

QCA6390 WiFi chip

Marvell 88E6393X Switch

512GB SATA SSD

eMMC 32GB

Customer feedback: Regardless of whether the fixed frequency is at 500MHz or the dynamic frequency is adjusted to 500MHz, the system will experience abnormalities, mainly manifested as PCIE communication abnormalities and RCU stall system freezing.


The customer wants an official response from NXP.

Re: LS1043AXN8QQB DVFS

Please refer to

https://community.nxp.com/t5/Layerscape/LS1043AXN8QQB-DVFS/td-p/2389683

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-04-2026 03:29 AM
更新者: