2389125_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2389125_en-US

2389125_en-US

MC33774 PWR voltage reading

HI.

I am currently using the MC33774 to read the voltages of the four AFEs: VAUX, VBAT, VDDC, and VDDA. I send two acquisition commands consecutively with a 10ms interval in between, and then send a read command after a 50ms wait to read the data from the SECM register. However, strangely, although the reads are correct most of the time, there are occasional cases where all the voltage values are very low. Why is this?

Embedded_novice_0-1782906617130.png

Embedded_novice_1-1782906700533.png


Re: MC33774 PWR voltage readingMy current sampling mode is APP mode, which caused a conversion error when reading these voltages (PER mode). After changing the sampling mode, the data acquisition is normal. Thank you for your help!Re: MC33774 PWR voltage reading

Hello Embedded_novice

Good day!

My first suspicion would be that the SECM supply-voltage results are being read before the measurement cycle has completely finished, or that the second acquisition command is restarting the conversion before the first result set is latched. This would explain why all four voltage channels become low together while communication itself remains functional.

  • Which acquisition command is being sent exactly?
  • Are the AFEs configured in periodic mode?
  • Do the low values occur on all four AFEs simultaneously, or only on one device in the daisy chain?
  • Can you try increasing the interval between acquisition commands?

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-02-2026 02:35 AM
更新者: