2388793_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2388793_en-US

2388793_en-US

i.MX8M Plus - WDOG_B# PU when using PCA9450C

Hi Team,

Do we need to mount 100k PU in WDOG_B# pin for using BSDL Mode?
As per Hardware Design Guide it says "If using a PMIC other than PCA9450, an external
pullup resistor (100 kΩ) may be required to support
Boundary-scan mode"

In EVK design it seems 100k PU was mounted in WDOG_B# pin they are using same PCA9450 PMIC.
Kindly confirm.

PMICRe: i.MX8M Plus - WDOG_B# PU when using PCA9450CAlthough PCA9450C disables WDOG_B reset by default and the pull-up is not strictly required for normal operation, NXP recommends adding the 100 kΩ pull-up when Boundary-Scan support is required. The EVK also populates this resistor to ensure a defined WDOG_B level during BSDL testing and avoid potential reset issues when WDOG_B is floating in Boundary-Scan mode.
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-02-2026 04:32 AM
更新者: