2387807_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2387807_en-US

2387807_en-US

Backward compatibility TJA1051

Hi,


i am using the TJA1050 in our products and replaced it with the TJA1051 because of this line in the datasheet:


Joern_0-1782742083202.pngJoern_0-1782742083202.png


Today i was working on another project and came across the TJA1051 again and saw this:


Joern_1-1782742158394.pngJoern_1-1782742158394.png


with Vio = VCC this means that VIH = 0,7*5=3,5V

From the datasheet TJA1050:

Joern_2-1782742224974.pngJoern_2-1782742224974.png


So in other words: TJA1050 and TJA1051 are not compatible on controller side.

Somehow i missed that part and now our products are running with the TJA1051 (not the /3 variant) directly connected to a Kinetis MK22, which has 3.3V outputs.

And it just works fine.


So my question is: am i lucky that it works?


Or is this a combination of the five volt tolerant MK22 pins and the internal pull up from the TJA1051 on TXD?

Joern_3-1782742390329.pngJoern_3-1782742390329.png


I am not sure on which way to go now...

Accept the fact that this is working or redesign all of our products?


Thanks in advance!


Greetings

Jörn


Re: Backward compatibility TJA1051

1:You can test the TX pin value during TJA1051 work.

2: change it into TJA1051/3,it should be no more risk.

Tags (1)
No ratings
Version history
Last update:
‎06-30-2026 02:29 AM
Updated by: