2387415_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2387415_en-US

2387415_en-US

S32K388 GMAC0 lwIP FreeRTOS S32DS36 RTD600 Debug Error

Dear

1. The original project was developed based on S32DS3.5 + RTD5.0.0, Build OK & Run OK

2. Development requires basic RTD 6.0.0. Development environment: S32DS 3.6.2 + RTD 6.0.0 + TCPIP_STACK_3.0.0 + FreeRTOS_11.1.0_6.0.0

3. RTD5.0.0 and RTD6.0.0 have significant differences, so projects based on the original RTD5.0.0 cannot be used. Instead, refer to the example code provided in the forum ( Example: S32K388 GMAC0 lwIP FreeRTOS S32DS 3.6.1 RTD600 ).

4. Modify the corresponding PIN according to your hardware platform as follows:

        

Ryan_xjl_0-1782662850043.png

5. Debugging the example code revealed that some initialization steps failed, as follows:

  

Ryan_xjl_1-1782662939895.png

6. If the corresponding code is masked, the program can run, but the PHY address cannot be found.

The attached file contains a debug example. I'm not sure if the reference example provided on the forum has been modified, or if I only modified the PIN definition, or if there's some other configuration error.


Re: S32K388 GMAC0 lwIP FreeRTOS S32DS36 RTD600 Debug Error

Hi, Petrs
Hello, you are absolutely right.
I am indeed using my own hardware platform. During RTD 5.0.0 debugging, I was able
to ping successfully using the example code provided on the official website. When using RTD 6.0.0 in person, I followed the same approach, mainly changing the PIN and discovering the code.The program failed to run. The attached file is based on my own hardware RTD 5.0.0 (S32DS3.5 + RTD 5.0.0 + TCPIP_STACK_2.0.0) and can ping.
The example code is OK, but I'm not sure if the clock configuration is incorrect. Could you please provide some assistance?

Re: S32K388 GMAC0 lwIP FreeRTOS S32DS36 RTD600 Debug Error

Hi,

It seems you only changed the MDIO/MDC pins compared to the community example you referred to.

Does this mean you are using your own custom-designed board?

I tested your project on the S32K388EVB-Q289, and the MCU initialization completed successfully.

The PHY address was not detected because the MDIO/MDC signals are connected to different pins on the EVB. After changing the MDIO/MDC pins to PTD16/PTD17, the PHY address was correctly obtained.

BR, Petr

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-01-2026 02:40 AM
更新者: