2387407_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2387407_en-US

2387407_en-US

S32k388 Boot ROM

There is mention of Boot ROM in the reference manual, but no further information is available.

RM just says five instances of 32kb boot rom is available 

At what point boot rom becomes relevant. Is there a firmware that run from here by the HSE even before sbaf is ran 

Re: S32k388 Boot ROM

Hi @Ars_,

Booting in managed by sBAF which is actually code in internal FLASH. These Boot ROM sections are for HSE use.

From an internal discussion, I can see that there was a request to modify the description, I will bump the thread to see when this fix will be applied.

Best regards,
Julián 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-30-2026 03:30 AM
更新者: