2387279_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2387279_en-US

2387279_en-US

S32K358 + FS2633: RSTB stays LOW with MCU assembled, but goes HIGH when JTAG is connected

I am using S32K358 with FS2633. When I test only the FS2633 section (MCU removed), the RSTB is released (HIGH) and the 3.3 V rail is present.

After assembling the MCU and all components, RSTB stays LOW, and the MCU does not boot.

If I connect a JTAG debugger, RSTB goes HIGH, I can successfully program the MCU, and the application runs normally. However, once I disconnect the JTAG, RSTB goes LOW again and the MCU stops running.

One observation is that the FS2633 RSTB output is a 3.3 V signal, while the S32K358 RESET line is pulled up to 5 V on my board. Despite this voltage difference, the system works correctly whenever the JTAG debugger is connected. Could this reset voltage level or the debugger be influencing the reset or power-up sequence?

Could this issue be related to the power-up sequence, reset timing, FS2633 startup configuration, or debugger-related behavior? Has anyone experienced a similar issue or have suggestions for debugging?

Re: S32K358 + FS2633: RSTB stays LOW with MCU assembled, but goes HIGH when JTAG is connected

You'd better try to test by pulling up the FS2633 RSTB to 3.3 V and check whether this issue has or not.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-30-2026 02:31 AM
更新者: