2387258_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2387258_en-US

2387258_en-US

CODEWARRIOR 11.1
I used a M9S08QG8 micro chip, with this code in 1984.
I am using windows 11 now.
Is there a compiler that will debug this code Now.
Also, is this chip still made?

void
my_main(void) { initial(); } void initial(void) { if(loopcount==2){goto initend;} PTADD_PTADD0 = 0; //io direction PTADD_PTADD1 = 0; PTADD_PTADD2 = 0; PTADD_PTADD3 = 1; PTBDD_PTBDD0 = 1; PTBDD_PTBDD1 = 1; //PTADD_PTADD4 = 0; //io direction //PTADD_PTADD5 = 0; //PTBDD_PTBDD6 = 1; //osc direction //PTBDD_PTBDD7 = 0; //PTBPE_PTBPE6 = 1; //pullup resistor //PTBPE_PTBPE7 = 0; //PTAPE_PTAPE0 = 0; //PTAPE_PTAPE1 = 0; //PTAPE_PTAPE2 = 0; //PTAPE_PTAPE4 = 0; //PTAPE_PTAPE5 = 0; //ICSC1_IREFS = 0; //select external osc param //ICSC1_CLKS0 = 0; //ICSC1_CLKS1 = 1; //ICSC2_EREFS = 0; //ICSC2_BDIV0 = 0; //ICSC2_BDIV1 = 0; PTAD_PTAD0 = 0; PTAD_PTAD1 = 0; PTAD_PTAD2 = 0; PTAD_PTAD3 = 0; PTBD_PTBD0 = 1; PTBD_PTBD1 = 1; bobbin_one_white=0; bobbin_two_white=0; bobbin_one_black=0; bobbin_two_black=0; bobbin_count_one=0; bobbin_count_two=0; bobbin_one_count_up_down = 20; bobbin_two_count_up_down = 20; bobbin_three_count_up_down = 20; bobbin_four_count_up_down = 20; rewind1 = 1; rewind2 = 1; rewind3 = 1; rewind4 = 1; programlength = 10; buzzcount = 0; buzzdelay = 0; buzzonoff = 1; needle = 20; delay = 100; light = 20; speed = 1000; c=0; //__RESET_WATCHDOG(); for(speed=0;speed<=1000;speed++){ PTAD_PTAD3=1;} //__RESET_WATCHDOG(); for(speed=0;speed<=1000;speed++){ PTAD_PTAD3=0;} //__RESET_WATCHDOG(); for(speed=0;speed<=1000;speed++){ PTAD_PTAD3=1;} //__RESET_WATCHDOG(); for(speed=0;speed<=1000;speed++){ PTAD_PTAD3=0;} PTAD_PTAD3 = 0; //buzzonoff = 1; buzzonoff = 0; initend: PTAD_PTAD3 = 1; //PTAD_PTAD3 = 0; c=0; peace(); } void peace(){ loopcount=2; onemoretime: buzzer(); //__RESET_WATCHDOG(); for(speed=0;speed<=delay;speed++){} if(PTAD_PTAD2==0){PTAD_PTAD3=0;buzzonoff=1;} //if(PTAD_PTAD2==0){setlength();} // winding bobbin on bobbin winder if(PTAD_PTAD0==0){bobbin_one_black++;PTBD_PTBD1=0;if(bobbin_count_one==1){bobbin_count_one=2;}} if(PTAD_PTAD0==1){bobbin_one_white++;PTBD_PTBD1=1;halfturna=1;bobbin_count_one=1;} if(bobbin_count_one==2){ if(halfturna == 1){fullturna=1;bobbin_count_one=0;}} // hook sewing if(PTAD_PTAD1==0){bobbin_two_black++;PTBD_PTBD0=0;if(bobbin_count_two==1){bobbin_count_two=2;}} if(PTAD_PTAD1==1){bobbin_two_white++;PTBD_PTBD0=1;halfturnb=1;bobbin_count_two=1;} if(bobbin_count_two==2){ if(halfturnb== 1){fullturnb=1;bobbin_count_two=0;}} if(fullturna==1)goto bobbinwinder; if(fullturnb==1)goto hook; goto onemoretime;
Re: CODEWARRIOR 11.1

Hello,

The CodeWarrior tool version 11.1, is supported in windows 11, this tool supports different connections [P&E USB Multilink Universal / USB Multilink, P&E Cyclone, Open-Source BDM, P&E Full chip simulation]

You can download the tool from this link: CodeWarrior® for MCUs (Eclipse IDE) v11.1

The device status is in "NOT RECOMMENDED FOR NEW DESIGNS (NRND)", but you can still order from the distributors available stock, please refer to product part page in buy options section MC9S08QG8CDTE Product Information | NXP Semiconductors

Best Regards, Luis

Tags (1)
No ratings
Version history
Last update:
‎06-30-2026 02:29 AM
Updated by: