2386463_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2386463_en-US

2386463_en-US

FEE INIT into hardware

Hello, I want to use FEE to store data, according to S32K344

屏幕截图 2026-06-25 215758.jpg

After configuring the example, during the init process, I entered the hardware. I tried unlocking the C40 beforehand, but it still didn't work. I used SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite. S32DS 3.6.3

 

Re: FEE INIT进hardware

Hi@ LJH1

I'll take some time next week to check it out for you.

回复: FEE INIT进hardware

It's not an NXP development board, it's the 8MHz board used by our hardware engineers.

Re: FEE INIT进hardware

The previous project was based on RTD 4.0.0, and maintenance and development primarily used this version. We will only switch to the new RTD version if we stop maintaining the old project, as the company needs a unified version.

Re: FEE INIT进hardware

Hi@ LJH1

I see that a total of two issues were created, both based on RTD 4.0.0.

I'd like to ask why we're still developing on this version. Our RTD version has already been updated to RTD 7.0.0, and many older versions...

The bug has been fixed in the new version. If possible, I recommend that you install and use the latest RTD version.

If for some reason I have to use RTD 4.0.0, then I will take some time to check the program you provided.

Also, I'd like to clarify what hardware you are using? I see in the project you provided that the external clock is set to 8MHz, which shouldn't be our NXP development board.

Re: FEE INIT进hardware

Hi@ LJH1

The pre-compilation options for the “MemAcc” component are incorrect.

Senlent_0-1782714638219.png


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-30-2026 02:32 AM
更新者: