I wanted to know the maximum power that is consumed by imx 95.
when i checked the Power tree in the EVK Schematic, it says VDD_SOC will use 14156mA, image attached
mrnobody_0-1782388613282.png
i felt this was too high, and as per their table imx95 soc itself uses 25 watts.
so i crosschecked it with the imx95 datasheet and there the same VDD_SOC is using 4400mA max, image attached
mrnobody_1-1782388839363.png
and not only this VDD_SOC line many other lines are also showing discrepancy, i would like to know which data is correct
Thankyou
Hello,
These values come from PI simulation is to verify the PCB performance to see if it meets the imx95 requirement, the spec in HDG is bases on the maximum current which list in EVK schematic.
The real current will NOT be that high, but we still recommend you use the maximum current to do the simulation and ensure it meets the requirement in NXP HDG.
The recommendation is use maximum supply currents from table 33 of datasheet in real use case scenario.
Best regards.