2386379_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2386379_en-US

2386379_en-US

How to Jump from App1 to App2 on the S32K344

Hi,

we are testing a custom jump from user App 1 to user  App 2 on the FRDM A S32K344

linker file of app1 and app2 is attached below 

#define APP_START_ADDRESS 0x00500000

void Bootup_Application(const uint32_t app_StarAddress)

{

uint32_t appEntry, appStack;

static void (*jump_to_application)(void);

/* Get the application's initial stack pointer value */

appStack = *((uint32_t *)(app_StarAddress));

/* Get the application's reset handler (entry point) address */

appEntry = *((uint32_t *)(app_StarAddress + 4));

/* Assign the application entry address to the function pointer */

jump_to_application = (void (*)(void))appEntry;

/* Relocate the interrupt vector table to the application */

S32_SCB->VTOR = (uint32_t)app_StarAddress;

/* Disable global interrupts (ASM_KEYWORD("cpsid i");) */

__asm volatile ("cpsid i" : : : "memory");

/* Set the Main Stack Pointer (MSP) */

__asm volatile ("MSR msp, %0\n" : : "r" (appStack) : "memory");

/* Set the Process Stack Pointer (PSP) */

__asm volatile ("MSR psp, %0\n" : : "r" (appStack) : "memory");

/* Jump to the application */

jump_to_application();

while (1)

{

/* Reaching here indicates an error occurred */

Siul2_Dio_Ip_WritePin(LED_RED_PORT, LED_RED_PIN, 1U);

}

}

Could you please verify Bootup_Application func can succeffuly jump to app2? If any additional steps are required, please let me know.

Re: How to Jump from App1 to App2 on the S32K344

Hi @ganavi1 


In principle, I can see no problem there. The only thing is that disabling of global interrupts may not be enough. I always recommend to de-initialize all used peripherals. Make sure that all interrupts are disabled also locally via peripheral registers, so they can’t be triggered again once global interrupts are enabled by App2.


Regards,

Lukas

Tags (1)
No ratings
Version history
Last update:
‎06-26-2026 02:34 AM
Updated by: