2386328_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2386328_en-US

2386328_en-US

kw47 lpuart

Hi:

Modify and verify the serial communication based on the official routine kw47loc_wireless_uart_freertos. Only modify Uart_RxCallBack and baud rate. The modifications are as follows: 

wjw2026_0-1782379752847.png

For the convenience of testing at present, 20 bytes are sent each time through the serial port. The test found that when the baud rate is lower than 256000, there are no problems with both receiving and sending. When the baud rate is set to 460800 or higher, the kw47 sends normally, but packet loss occurs during reception. 

Could you please check if I'm using it improperly and give me some guidance? 

Also, why is there no kw47loc_freertos_lpuart_cm33_core0 routine in sdk_26_03_00? 

Thank you! 


Tags (1)
No ratings
Version history
Last update:
‎06-26-2026 02:36 AM
Updated by: