Hello,
While evaluating the new version of the DDR configuration for the i.MX95, I came across what looks like a bug in the configuration tool.
Here is exactly what I did, so the behavior can be reproduced:
1. Installed the Linux version of the tool.
2. Created a new configuration.
3. Selected processor MIMX9596xxxxN.
4. Changed the preset to "LPDDR4X EVK / FRDM 15x15 4000MTs Configuration".
5. Saved the configuration, then closed the tool.
6. Reopened the tool and loaded the saved configuration.
At that point the DDR configuration is not displayed at all.
At least the 26.03 version was starting with MCU unselected (selecting it manually solves the problem), now there is no way to solve the problem.
Thank you very much for your help.
Best regards,
Emanuele
Also the windows version of the tool shows the same problem.
Attached screenshots.
Hello,
Thank you for report this bug in the tool.
I was able to see the issue on my side.
I will report it with internal team to solve it as soon as possible.
Best regards.
Is there an update or a workaround? It is impossible to use it
I've just installed and tested version 26.09. Followed the same steps that Emanuele listed but for MIMX9529xxxxx.
The incorrect behavior is the same, impossible to load previously created config files.
Tested on Ubuntu 24.04.
Best regards,