2384993_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2384993_en-US

2384993_en-US

Brake Control Monitoring Course Using NXP FRDM-A-S32K3 Automotive Platforms

Introduction

Braking systems are among the most important safety-related functions in modern vehicles. Modern automotive electronic systems continuously monitor brake inputs and react in real time to ensure driver awareness and vehicle safety.

This course introduces brake control and brake status monitoring concepts using NXP S32K3 automotive microcontrollers and Application Code Hub examples. Through practical demonstrations, participants will learn how embedded software acquires, processes, and reacts to brake-related signals using automotive-grade development platforms. The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.

The course is based on the following Application Code Hub demonstrations:

Both examples implement the same brake monitoring concept and can be executed on either FRDM-A-S32K312 or FRDM-A-S32K344, allowing teachers, students, and developers to choose the platform that best fits their hardware availability and learning objectives. The demonstrations simulate a braking event using a Force Click board connected through the FRDM K64 Click Shield. The Force Click acts as a brake pedal sensor and generates an analog signal proportional to the applied pressure. This signal is acquired through the MCU ADC peripheral, processed by the application, and used to drive a 4x4 RGB Click board that provides visual indication of the current braking condition. The examples illustrate how automotive brake monitoring systems can detect braking events and react in real time using embedded software running on the S32K3 platform.

FRDM-A-S32K312FRDM-A-S32K312FRDM-A-S32K312FRDM-A-S32K344FRDM-A-S32K344FRDM-A-S32K344

Course Objectives

After completing this course, participants will be able to:

  • Understand the fundamentals of automotive brake monitoring systems
  • Acquire analog signals using ADC peripherals
  • Process brake-related inputs in real time
  • Control visual indicators based on system status
  • Understand ADC and FlexIO peripheral integration
  • Develop applications using S32 Design Studio and RTD drivers
  • Prototype automotive applications on FRDM-A-S32K312 and FRDM-A-S32K344 boards

Hardware Platforms and Components

Platform Selection

One of the advantages of this course is the flexibility to use either the FRDM-A-S32K312 or the FRDM-A-S32K344 platform. Both examples demonstrate the same automotive brake monitoring functionality and learning concepts, enabling users to select the board available in their laboratory environment while following the same workflow and development methodology.

FRDM K64 Click Shield

Provides mikroBUS™ connectivity for Click boards and simplifies hardware expansion.

Force Click

Simulates the brake pedal input by generating an analog signal proportional to the applied pressure. The ADC peripheral continuously reads this signal to determine the brake status.

4x4 RGB Click

Acts as the brake status indicator. Different LED patterns can be used to represent braking conditions and emergency braking events. The LEDs are controlled through the FlexIO peripheral.

Brake Control Monitoring on FRDM-A-S32K312Brake Control Monitoring on FRDM-A-S32K312Brake Control Monitoring on FRDM-A-S32K312Brake Control Monitoring on FRDM-A-S32K344Brake Control Monitoring on FRDM-A-S32K344Brake Control Monitoring on FRDM-A-S32K344

System Architecture

The application follows a simple automotive workflow:

  1. The user applies pressure to the Force Click sensor.
  2. The ADC peripheral acquires the analog value.
  3. The application processes the braking signal.
  4. Brake status is evaluated against predefined thresholds.
  5. The 4x4 RGB Click LEDs are updated to indicate the current braking condition.

This workflow illustrates how sensors, software processing, and output indicators interact in a real-time automotive embedded system.

ramonadragulin_5-1782210701819.pngramonadragulin_5-1782210701819.png

Educational Value

This course can be used as:

  • Eat-Sleep-Code-Repeat University laboratory material
  • Automotive embedded systems training
  • S32K3 hands-on workshop content
  • Introduction to automotive safety-related software
  • Application Code Hub learning path

Students gain practical experience with ADC acquisition, signal processing, real-time decision making, and peripheral control using real automotive hardware.

Getting Started

  1. Open S32 Design Studio.
  2. Select Import Project from Application Code Hub.
  3. Search for the desired brake demo.
  4. Import the project.
  5. Build and flash the application.
  6. Assemble the hardware.
  7. Apply pressure on the Force Click sensor.

Observe the brake status indication on the 4x4 RGB Click LEDs.

Conclusion

This course demonstrates how brake control and brake status monitoring systems can be prototyped on NXP S32K3 automotive platforms. By combining analog signal acquisition, real-time processing, and LED-based indication, the examples provide a practical introduction to automotive embedded software development and safety-oriented system design. Participants can choose either the FRDM-A-S32K312 or FRDM-A-S32K344 platform and follow the same learning path to understand the implementation of brake monitoring functionality on modern automotive microcontrollers.

Result on FRDM-A-S32k312Result on FRDM-A-S32k312Result on FRDM-A-S32k312Result on FRDM-A-S32K344Result on FRDM-A-S32K344Result on FRDM-A-S32K344

References

Tags (1)
No ratings
Version history
Last update:
‎06-23-2026 04:36 AM
Updated by: