I am currently using the S32K3X8EVB-Q289 evaluation board and have developed a custom hardware design based on the S32K358 MCU.
Could you please clarify:
Thank you for your support.
Regards,
Yash Gupta
Hello @Yash2530 ,
1. Yes, using the S32K3X8EVB-Q289 on-board debugger to program/debug an external S32K358 target is supported. Actually, the EVB’s on-board OpenSDA debugger uses a P&E Micro-developed bootloader/debug application - https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715877
2. No soldering rework or jumper setting is required on the EVB for this use case.
3. J55 USB host connector.
4. In practice, for standard flashing and source-level debug of an external S32K358 target, the EVB’s on-board debugger should be sufficient. Since I don't know what feature is important to you, please compare features by yourself:
https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=5045
5. Yes, https://www.nxp.com/webapp/Download?colCode=S32K3X8EVB-Q289HWUM
Best regards,
Pavel
@PavelL ,
Got this error while trying to program my external controller.
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 00400000-0042F4B7 ...
Calculated CRC-16 does not match block. (File = $A9EE, Device = $EDEF)
Error verifying flash of device
Error occured during Flash programming.
INFO: DAP IDCODE = 0x6BA02477
INFO: DAP successfully powered up. DP CTRL/STAT = 0xF0000000
Starting reset script (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac) ...
REM Enable clocks for selected cores in MC_ME module
Delaying for 200mS ...
Done.
REM Initialize RAM and DMA:
REM Initialize DMA TCD:
REM Copy valid executable code to RAM for each core to be used.
REM Enable required cores in MC_ME:
Delaying for 20mS ...
Done.
Delaying for 20mS ...
Done.
Reset script (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac) completed.
PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.
PE-ERROR: Error downloading to the device. Terminating debug session.
Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "53100" from 6224
PE-ERROR: Error : Attempted to send response but connection already closed.
Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "53104" from 7224
INFO: DAP IDCODE = 0x6BA02477
Target Disconnected.
Yash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpegYash2530_0-1789183717483.jpeg
Please help me resolve these.
Regards,
Yash Gupta
Hello @Yash2530 ,
I performed a reference test using an S32K3X8EVB-Q289 and the on-board PEmicro debugger connected through J55.
In my test, the first CRC verification also reported a mismatch because the existing flash content was different from the application being downloaded. However, the programming sequence then continued with flash erase and programming. Therefore, the initial CRC mismatch is not necessarily the root cause and does not, by itself, confirm that Secure Debug is enabled.
The important difference is that, in the log you provided, the debug session terminates immediately after the first VC command. I do not see the subsequent EM and PM commands for erasing and programming the flash.
Please check the PEmicro debug launch configuration, particularly whether downloading the executable and flash programming are enabled. Please also provide the complete PEmicro log from the beginning of the session. The beginning of the log should show the CM command and the selected .arp flash algorithm.
For reference, my successful test used the following algorithm for an HSE-disabled device:
PavelL_0-1789370094591.pngPavelL_0-1789370094591.pngPavelL_0-1789370094591.pngPavelL_0-1789370094591.pngPavelL_0-1789370094591.png
BTW, please create a new thread next time - we actively tracked community threads only 7 days after last answer. I only receive subscription emails for updates and those can occasionally be missed.
Best regards,
Pavel
Hello @PavelL ,
I have programmed the device issue was with the Reset pin of JTAG conflicting with Onboard MCU and Target board MCU. So I isolated reset pin from JTAG RESET pin and programming works. Now only issue I have to reset the mcu manually.
Have you also used a custom target along with EVK board jtag( J50 & J55(usb)) connectors.
Regards,
Yash Gupta
Hello @Yash2530 ,
Yes, I have used both an external PEmicro debugger and Lauterbach TRACE32.
According to my notes, all jumpers on the EVB were kept in their default positions, except for J685 and J23, which were set to positions 2-3.
For your reference, the jumper configuration was as follows:
With this configuration, programming, debugging and automatic reset worked correctly in my setup. Please compare these jumper settings with your current EVB configuration.
Best regards,
Pavel
Hello @Yash2530 ,
" provide i2c and spi example code" is a new topic. To keep clarity of threads, please create a new, dedicated thread.
Thank you for your understanding.
Best regards,
Pavel
@PavelL ,
Thanks for your response that really helped, can you also share i2c and spi example code as the RTD ones contains loop back examples, as I have tried to initialise my peripherals over spi and i2c by keeping them master, but I have no clock signal over sck in both not mosi and miso also responding. That would really help if you share one.
Thanks,
Yash Gupta