Hi,
Going through the AN14449 document, I cannot find the temperature condition for the measurements? Was the heat-sink mounted? Was the fan mounted and running? What ambient temperature was used?
Hello,
The board was tested as it is.
Oswalag_0-1782841642133.png
The Note: In the used BCU software tool, measurements are performed using the on-board measurement circuitry
and these measurements are taken at room temperature without thermal forcing equipment. Only means it was tested on ambient temperature, it wasn't tested in a chamber room but the board keeps the heatsink and fan.