2383704_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2383704_en-US

2383704_en-US

S32K314 UART

I recently encountered a problem while debugging the S32K314 serial port. Previously, I was using the GD32/STM32 platform, and when using the serial port for real-time printing, my approach was as follows: the application layer processed the printed characters, and the underlying write function was called to send them out via interrupt.

Joker_Y_2-1781951653320.pngJoker_Y_2-1781951653320.png

Joker_Y_4-1781951712695.pngJoker_Y_4-1781951712695.pngJoker_Y_5-1781951735385.pngJoker_Y_5-1781951735385.png


This data is written directly to the data register and sent out quickly. Therefore, there's no need to panic when the application layer receives a large amount of data, as there's a queue, and data transmission is fast. However, when using S32K3, I found that the asynchronous send function `Lpuart_Uart_Ip_AsyncSend` is relatively slow, with nested layers. Relatively speaking, for the same number of bytes of printed data, S32K3 is much slower than GD32. AI provides a solution.

Joker_Y_6-1781952019622.pngJoker_Y_6-1781952019622.png


In the application layer, the write-by-write method is changed to writing to the underlying layer using a large buffer. Then, the underlying write function and interrupt are handled in the following way.

Joker_Y_7-1781952213976.pngJoker_Y_7-1781952213976.png

Joker_Y_8-1781952251883.pngJoker_Y_8-1781952251883.png

This method does improve speed, but it requires a lot of RAM. Is there a better way that is better in terms of both space and efficiency?




Re: S32K314 UART

do you use any operating system at MCU level or just baremetal?

Re: S32K314 UART

Operating system used

Re: S32K314 UART

Hi@ Joker_Y

If possible, you can try to implement LPUART transmission directly using registers.

Re: S32K314 UART

Could you please provide an example of how to do this?

Tags (1)
No ratings
Version history
Last update:
‎06-27-2026 03:30 AM
Updated by: