The S32K3XX reference manual talks about the "drive-strength enable" bits, but doesn't appear to define what this means - the closest reference I can find is that it seems correlated with maximum frequency supported by certain pins (page 42 of the S32K3XXRM/Section 4.4.1)
Is there something explicit in terms of maximum current draw or other things I should be aware of for why I should or should not enable "drive-strength"?
GPIO-Standard: Switching up to 10 MHz High drive-strength not supported. Slew-rate control not supported.
—
GPIO-Standard plus: Switching up to 25 MHz Supports high drive-strength. Slew-rate control not supported.
—
GPIO-Medium: Switching up to 50 MHz Supports high drive-strength. Supports slew-rate control.
—
GPIO-Fast: Switching up to 120 MHz Supports high drive-strength. Supports slew-rate control.
Hi
The S32K3XX Reference Manual (S32K3XXRM) states that the Pad Type "GPIO-Standard" does not support high drive strength, whereas "GPIO-Standard Plus", "GPIO-Medium", and "GPIO-Fast" support high drive strength.
For GPIO Pad Type, please refer to the S32K344_IO Signal Table, specifically column H, in the Excel attachment S32K344_S32K324_S32K314_IOMUX.xlsx provided with the S32K3XXRM.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
As I told the previous poster, I know which pins do and do not support "high drive strength," that is not the issue!
But fortunately, in the background you had the relevant chunk of information: in S32K3xx.pdf, Table 27. GPIO DC electrical specifications, appears to have what I need.
It looks like it doubles the output current of the pins to enable the "DSE = 0" vs "DSE = 1"