2383411_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2383411_en-US

2383411_en-US

LX2160A XSPI in Single Mode - Unused pins

HI,

It is not clear what would be the configuration of the DAT2-DAT7 signals when configuring the XSPI to operate in a Singl Mode.

Can they be left unconnected?

Noam

Re: LX2160A XSPI in Single Mode - Unused pins

Hi,

The thing is that pins are configured in groups, in particular:

XSPI1_A_DATA30_PMUX: configures XSPI_A_DATA[3:0] for either SPI or GPIO

Is it still safe to leave DAT[3:2] floating when using single mode spi?

Re: LX2160A XSPI in Single Mode - Unused pins

Hello,

On LX2160A XSPI Single mode, DAT2–DAT7 may be left unconnected, with the documented recommendation that unused XSPI data pins be configured as GPIO outputs and left as no-connect.


Regards

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-23-2026 02:39 AM
更新者: