2383273_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2383273_en-US

2383273_en-US

Mac OS Tahoe update LinkServer No Probes found

So I updated to Tahoe and the probes were not found when using LinkServer.  So I updated LinkServer to latest but it only works if I go into the directory in terminal and manually run 

./LinkServer probe

After that the probe is found and I can use MCUXpresso.  This apparently happens to others as well.  
https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-not-found/m-p/2200131/highlight/true#M5741

This is the error in the IDE when it tries to use LinkServer

redlink> ProbeList

Error: No probes found



I also work at a large company and others who have updated their OS have the same issue and have to do the same thing.  

Anyone know of a better fix?

Re: Mac OS Tahoe update LinkServer No Probes found

Hi @davidinsulet,

Unfortunately, that's a current limitation of the LinkServer build that comes preinstalled on the latest version of MCUXpresso IDE. That said, this limitation has been identified and reported with the IDE team so they can correct the LinkServer version on a future release.

On the meantime, the workaround that is described on the post you shared is the most effective method of getting around this issue specifically for MCUXpresso IDE.

Alternatively, you would also recommend using MCUXpresso for VS Code, which is our newest development platform and doesn't currently have this limitation like the IDE does.

Sorry for the inconvenience this may cause.

BR,
Edwin.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-25-2026 02:33 AM
更新者: