2383150_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2383150_en-US

2383150_en-US

IW610 - WLAN Activity Indicator

Just a quick question, is there any GPIO pin/functionality which could be "misused" as WLAN activity indicator (blinking/toggling with WLAN traffic) to power a LED?

There is no dedicated function for this as far as I could see and the idea to use the HOST WAKE UP functionality for it doesnt work, because it is only enabled when the host really is asleep.

Re: IW610 - WLAN Activity IndicatorThank you, that is what I got from the documentation too, but wanted to ask if I had overlooked something.

Falsely I believed the HOST WAKE UP could be misused because it can generate events for incoming data. But that GPIO signal is only available if the Host is actually asleep, so it's not usable either.
Re: IW610 - WLAN Activity Indicator

Hello,


Hope you are doing well. There is no GPIO or alternate pin function intended to indicate general WLAN traffic/activity. The available GPIO functions are standard interfaces, coexistence signals, reset, and wake/interrupt signaling.

The practical implementation would need to come from the host side (for example, software-driven LED control based on driver/network activity).


Best Regards,

Ricardo

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-19-2026 03:27 AM
更新者: