2382693_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2382693_en-US

2382693_en-US

Choosing an MPU for PXI controller

I want to create an open-source PXI chassis controller (if someone doesn't know, it's basically an ARM SBC, connected to backplane via PCIe, peripheral PXI modules do the same, but have PCIe EP instead of RC)

So, I need an MPU that can run linux distr, e.g. Ubuntu, in graphic mode with decent performance, as some specialised software would be running on it, e.g. LabVIEW and custom peripheral modules control utilities, that process Gbs of raw data per second. It should also have at least 2 independent PCIe RCs, as denanded by PXI spec, and the faster they are the better: if they are fast enough, it would be possible to e.g. feed DAC in RF AWG with raw data continuously, not limited by AWG ram size. Also a possibility to connect a lot of LPDDR4 would be cool, not just typical 32 bit bus, but 64+

The new TI Am69a looks like a cool thing, but it seems like it's going to cost a lot, and it's very new, so no full errata, no software examples, drivers and so on - looks too challenging for me, being a hardware developer and coding only as hobby

Another way would be Rockchip RK3588, it's more affordable and older, but it's PCIe is too slow, just 2x2 gen 3. I could definitely live with it, but... Maybe you have better ideas or done something similar recently? Would be grateful to hear them

Re: Choosing an MPU for PXI controller

You may consider LS1046A or LX2160A. However, these SoCs do not integrate a graphics engine for GUI, so an external solution (for example, remote GUI or a discrete GPU) would be required.

Thanks.

标记 (1)
无评分
版本历史
最后更新:
‎06-18-2026 04:27 AM
更新人: