2382341_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2382341_en-US

2382341_en-US

BT HF is not working by using NXP sd8987 wifi+BT combo module in android OS

Hi,

I am using NXP chip sd8987 (M2-JODY-W263-10C) with TI soc am62p. I am using android OS. a2dp is working, but hands free is not working. I have only 1 codec speaker.
is there anything to be taken care from the pin perspective of M2-JODY-W263-10C (sd8987) module.

Regards

Roshan

Re: BT HF is not working by using NXP sd8987 wifi+BT combo module in android OS

Hi, @Roshan888 

Can you please let me know what is your Android version?

Did you use PCM/I2S interface for SCO on SD8987 M2-JODY-W263-10C module?

Could you please provide me a full log from booting up your device and including the full A2DP connected but HFP could not work process?


Best regards,

Christine.

Re: BT HF is not working by using NXP sd8987 wifi+BT combo module in android OS

Hi Christine,

I'm not using the pcm/i2s pin. Software HFP path over UART.

I'm using TI am62p soc android version 16. 
Attached the bluetooth_manager log.

Regards

Roshan

Re: BT HF is not working by using NXP sd8987 wifi+BT combo module in android OS

Hi, @Roshan888 

Thanks for your dumpsys and your information.

From your dumpsys, I see that the RFCOMM is already opened, and SCO is created successfully, also the handler has already been initiated.

To debug further, can you please help to provide me:

1.Bluetooth HCI snoop log including the whole process including the full connection, A2DP connected but HFP could not work process?

On Android, you can capture HCI logs by enabling Bluetooth HCI snoop log in Developer Options , toggling Bluetooth once to start capture, and then exporting the log with adb .

Steps:

  1. Open Developer Options
  2. Enable Bluetooth HCI snoop log
  3. Toggle Bluetooth off and on once
  4. Trying to reproduce the issue.
  5. Pull the log file with ADB commands.

2.

adb shell dumpsys media.audio_policy > audio_policy.txt
adb shell dumpsys media.audio_flinger > audio_flinger.txt
adb logcat -b all -d > logcat_log.txt (from booting up your device)
 
Best regards,
Christine.

Re: BT HF is not working by using NXP sd8987 wifi+BT combo module in android OS

Hi, @Roshan888 

Can you please help to provide the requested logs to move forward on this issue?


Best regards,

Christine.

Re: BT HF is not working by using NXP sd8987 wifi+BT combo module in android OS

Hi, @Roshan888 

Does your issue resolved?

Do you still need our support? 

If yes, can you please help to provide the requested logs to move forward on this issue?


Best regards,

Christine.

Tags (1)
No ratings
Version history
Last update:
‎07-03-2026 02:28 AM
Updated by: