2382268_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2382268_en-US

2382268_en-US

IMX8MPLUS - Bit rate variations for H.264/2656 coded Video stream from Camera

Hi,

I am using NXP i.MX8Mplus for a camera module product. I use two cameras, one on USB and second on MIPI-CSI2 interfaces. The data path looks like:

Camera sensor -> MIPI-CSI -> ISP (bypassed, just DMA) -> GPU (OSD) -> VPU  (h/w encoder) -> RTSP stream on ethernet.

I set my bit rate for encoded video stream to 4 Mbps. The pipeline setup looks like this:

gst-launch-1.0 -v \
v4l2src device=/dev/video2 io-mode=dmabuf ! \
video/x-raw,format=NV12,width=1920,height=1080,framerate=30/1 ! \
vpuenc_hevc bitrate=4000 gop-size=60 ! \
h265parse config-interval=1 ! \
fakesink sync=false

Problem: The customer reports that bitrate varies a lot, the variation is +/- 50%, sometimes even peaks to 100%.  Expectation of customer is variation must be capped to 20% max.

How can we achieve this, i saw that CBR is not supported in SDK i am using on IMX8Mplus. I am using Yocto SDK , old one 'mikeldore' branch:

repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-mickledore -m imx-6.1.55-2.2.0.xml


Please le us know:

- if it is possible to lessen the variation to 20%, if yes how?


Thanks

pankaj


Re: IMX8MPLUS - Bit rate variations for H.264/2656 coded Video stream from Camera

i.MX95 does support encoder constant-bitrate control for H.264/H.265 through V4L2, but “steady bitrate” should be understood as CBR target control rather than perfectly fixed instantaneous output.

Re: IMX8MPLUS - Bit rate variations for H.264/2656 coded Video stream from Camera

Thank you for the reply Yiping.  I am trying these suggestions now. One more question, what about IMX95 , does encoder in IMX95 support steady bitrate?


thanks

pankaj


Re: IMX8MPLUS - Bit rate variations for H.264/2656 coded Video stream from Camera

Yes, you can reduce the variation, but:

  • Achieving strict ±20% bitrate on i.MX8MP VPU is NOT guaranteed
  • You can realistically reduce it from ±50–100% → ~±20–40% with proper tuning
  • True CBR requires:
    • v4l2-based encoder (v4l2h264enc / v4l2h265enc)
    • explicit rate-control + QP constraints

 

 Step 1 — Switch to V4L2 encoder (critical)

Replace:

vpuenc_hevc

with:

v4l2h265enc

Step 2 — Enable real rate control + CBR mode

gst-launch-1.0 -v \

v4l2src device=/dev/video2 io-mode=dmabuf ! \

video/x-raw,format=NV12,width=1920,height=1080,framerate=30/1 ! \

v4l2h265enc extra-controls="encode, \

frame_level_rate_control_enable=1, \

video_bitrate_mode=1, \

video_bitrate=4000000, \

h265_min_qp=20, \

h265_max_qp=30" ! \

h265parse config-interval=1 ! \

fakesink sync=false


Step 3 — Tune QP range (MOST IMPORTANT)

Setting

Effect

Wide QP (e.g. 10–51)

large bitrate variation

Narrow QP (e.g. 20–30)

lower variation, lower quality

Very narrow (e.g. 24–28)

near-CBR behavior

For the requirement:

  • Start with: QP range = 20–30
  • If still >20% variation → tighten to 22–28
  •  

Step 4 — GOP / I-frame control

Your current:

gop-size=60

Issue:

  • I-frame causes large spikes (2–5x bitrate)

gop-size=30 (shorter GOP helps)

Mitigation:

OR (better):

  • Enable intra-refresh (if supported)
  • Avoid large IDR spikes

Step 5 — Optional smoothing (network level)

Even after encoder tuning, short bursts may remain.

Add:

  • queue + rtpjitterbuffer
  • OR socket buffer shaping

This smooths network bitrate, even if encoder fluctuates.

Tags (1)
No ratings
Version history
Last update:
‎06-18-2026 02:27 AM
Updated by: