2382262_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2382262_en-US

2382262_en-US

RTD Import in S32 Design Studio for S32 Platform issue

The main issue I'm facing in S32 Design studio is while integrating .c and .h files,if i create a project and select from project explorer,sdk is not showing any versions,then the next issue is in config tools,i,e  it shows MCU is not selected.Even after importing RTD from external,no MCU is being selected.Not able to select project also in this tool.

Re: RTD Import in S32 Design Studio for S32 Platform issue

Hi

Please refer to the instructions in the video(How To Download, Install and Configure the RTD 5.0.0 with S32 Design Studio 3.6.0) to download and install the specific version of S32K3 RTD that you need. The latest version has been updated to S32K3 RTD 7.0.1.

And don't forget to install NXP GCC for Arm Embedded Processors v10.2 build 1728


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

标记 (1)
无评分
版本历史
最后更新:
‎06-18-2026 02:28 AM
更新人: