2382019_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2382019_en-US

2382019_en-US

S32K312 mini board is not available

S32K312 mini board is not available in example code of S32 design studio 3.6.  I have installed all the drivers as well. Kindly help me out.

Re: S32K312 mini board is not available

Hi @Turtledove 

Based on the screenshot you shared, it appears that no software packages are currently installed.

The RTD for S32K3 devices can be downloaded from S32K3 Standard Software, under:
Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M. Once downloaded, it can be installed following the steps described in the thread How To Download, Install and Configure the RTD 5.0.0 with S32 Design Studio 3.6.0.

Regarding examples for the FRDM-A-S32K312, there are currently no examples specifically provided for this board within the RTD package. Also, in the most recent release, there are no dedicated examples for the S32K312 device. However, you can still use examples from other S32K3 derivatives as a reference.

Although examples are not provided within the RTD packages, application examples for the FRDM-A-S32K312 are available in the Application Code Hub. You can search for this specific device there, and all available examples will be displayed.
 
BR, VaneB
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-17-2026 02:32 AM
更新者: