Hello! I'm following the "Start Building With MR-CANHUBK344s" post as a getting started project to test the capabilities of the MR-CANHUBK344 board since it is exactly what I need for an automotive on-going project.
Te project as-is does not compile and could not be loaded into the board. The dependencies needed for the out-of-box project are as follows:
I have unsuscessfully tested a couple of setups already with current and previuos software versions like:
Both with different versions of RTD drivers, and S32Kxx development package versions and also different FreeRTOS version.
From the get-go the main issue is that the dependencies needed are no longer suported on new software versions and also the dependencies specified on the getting started document are no longer available to download from NXP's website.
Could NXP provide the required dependancies for a local test of the IEEE1722 bridge getting started example or is the manual porting the only option to follow if I need to test that specific app?
Hi @Mianromo
Could you please help me check if, on the page where you download the FreeRTOS update site for S32DS, there is a “Previous” tab available? If yes, could you also take a look and let me know if you can see the SW32K3_FreeRTOS_10.4.6_2.0.0_D2204 package listed there?
BR, VaneB
Hello @VaneB,
Does the "Escalate" button works the same as requesting a Support Ticket?
Best Regards,
Hi @Mianromo
Could you please help check if you are able to access the desired software version through this link?
Note: Before accessing the link, please make sure to log in to flexnetoperations. You can do this via My NXP Account → Software Licensing and Support → Software Accounts.
If no, please submit a support ticket so we can provide you with further assistance.
Hello @VaneB,
This is where I am looking for that specific file that is being mentioned in similar post regarding the same issue: https://nxp.flexnetoperations.com/control/frse/product?child_plneID=833477#
On that webpage several versions for the FreeRTOS package are available for download but that one you mention is not listed. The "Previous" tab is shown but it is grayed out and unclickable. Attached image is for reference.
The other packages that are needed for the "Start Building With MR-CANHUBK344s" guide were downloaded from their respective previous tab but I'm missing the FreeRTOS one for it to compile as-is.
Best regards,
Hello @VaneB,
The link you provided sent me to this url: https://www.nxp.com/mynxp/profile
I made sure to be logged in before clicking on it. I guess the only option would be the support ticket.
Best regards,
Hi @Mianromo
Thank you for your help in submitting the ticket. I have already replied to you through that channel.