2380570_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2380570_en-US

2380570_en-US

Falcon Mode Enablement - iMX8MP_EVK

Hi,
I need to enable Falcon Mode on iMX8MP_EVK in the Yocto branch 6.12-walnascar. However, as per the AN14641 document, the meta-imx-fastboot layer is available only in the lf-6.6.36-2.1.0-secure branch. How can I port this layer to my walnascar branch and enable Falcon Mode?
Please help here..

Re: Falcon Mode Enablement - iMX8MP_EVK

Please use the following command.

uuu -b emmc_all -.rootfs.wic

For example:

$ uuu -b emmc_all imx-boot-imx95evk-sd.bin-flash_all     core-image-minimal-imx95evk.rootfs.wic

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi Tipingwang,

Thanks for your reply.

I am trying to enable Falcon mode and have followed the steps provided in AN14641, but I am getting stuck during the flashing process.

As per the README, the flashing steps are mentioned as below (for eMMC):

unzstd -[secure-boot]-.rootfs.wic.zst
uuu -b emmc_all -.rootfs.wic
uuu -b emmc

My boot memory is eMMC. I attempted to flash the image using the following command:

sudo ./uuu -d -v -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-core-imx8mpevk.rootfs-20260616051114.wic

However, during execution, the flashing process fails with the following error:

sudo ./uuu -d -v -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-core-imx8mpevk.rootfs-20260616051114.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-5-g124d086
 
Build in config:
Pctl Chip Vid Pid BcdVersion Serial_No
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDPS: MX93 0x1fc9 0x014e
SDPS: MX91 0x1fc9 0x0159
SDPS: MX95 0x1fc9 0x015d
SDPS: MX95 0x1fc9 0x015c
SDPS: MX943 0x1fc9 0x0027
SDPS: MX952 0x1fc9 0x0028
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152
FB: 0x0483 0x0afb
FB: 0x1d6b 0x0104
 
Run built-in script:
 
uuu_version 1.4.149
 
# @_flash.bin            | bootloader, which can extract from wic image
# @_image   [_flash.bin] | wic image burn to emmc.
 
 
# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000
 
# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -scanterm -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000
 
# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mpevk-sd.bin-flash_evk -offset 0x57c00
SDPU: jump -scanlimited 0x800000
# }
 
# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mpevk-sd.bin-flash_evk -skipspl -scanterm -scanlimited 0x800000
SDPV: jump -scanlimited 0x800000
# }
 
 
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all imx-image-core-imx8mpevk.rootfs-20260616051114.wic
FB: flash -scanterm -scanlimited 0x800000 bootloader
imx-boot-imx8mpevk-sd.bin-flash_evk
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done
 
 
Wait for Known USB Device Appear...
New USB Device Attached at 1:2-152E1000D9DE520A
1:2-152E1000D9DE520A>Start Cmd:SDPS: boot -scanterm -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000
14%1:2-152E1000D9DE520A>Fail HID(W): LIBUSB_ERROR_TIMEOUT (-7)(20.07s)

The detailed uuu logs are attached above for reference.

Could you please guide me on the correct procedure to flash a Falcon-enabled OS into eMMC, or let me know if I am missing any required steps or configurations?

Thanks in advance for your support.

Re: Falcon Mode Enablement - iMX8MP_EVK

Falcon Mode is not incompatible with Secure Boot
BUT
On lf-6.12.20-2.0.0-secure, you cannot enable Secure Boot together with Falcon Mode using the provided Yocto flow


About 0001-imx8m-reset-ethernet-phy-in-spl.patch

For i.MX8MP EVK → strongly recommended

Not strictly required if you don't use Ethernet during early boot

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi Yiping Wang,
Thank you for your response.
I have a couple of additional questions for clarification. According to the information provided, the branch lf-6.12.20-2.0.0-secure supports Falcon Mode v2, but Secure Boot is marked as not yet supported.

Since Secure Boot is a requirement for my i.MX8MP platform, will Falcon Mode work correctly if I use this branch, or is Falcon Mode incompatible when Secure Boot is enabled?

For the i.MX8MP EVK, do I need to apply the patch 0001-imx8m-reset-ethernet-phy-in-spl.patch, or is it optional depending on the use case?

Re: Falcon Mode Enablement - iMX8MP_EVK
You probably do not need to port the layer from lf-6.6.36-2.1.0-secure yourself. The public nxp-imx-support/meta-imx-fastboot - GitHub repository already shows a lf-6.12.20-2.0.0-secure branch.
Re: Falcon Mode Enablement - iMX8MP_EVKPlease help here,
And i am using UUU to flash eMMC
Re: Falcon Mode Enablement - iMX8MP_EVK

Screenshot from 2026-06-16 14-28-09.png

As per this image i found in NXP forum it seems that flashing eMMC using the UUU tool may not be supported in this case. Could you please suggest the appropriate method to flash an eMMC device with a Falcon-enabled OS?

In your previous reply, you suggested using the following command:
 -.rootfs.wic>


I tried this approach, but I encountered the same error again:
Fail HID(W): LIBUSB_ERROR_TIMEOUT (-7) (20.07s)
Could you please guide me on the correct flashing procedure or any alternative tools or steps required for flashing eMMC with Falcon mode enabled?


Re: Falcon Mode Enablement - iMX8MP_EVK

I verified the following commands on IMX95FRDM, there is no problem, please refer to my log.

C:\Users\nxa22585>C:\Users\nxa22585\Downloads\i.mx95\uuu.exe -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion Serial_no
====================================================================
2:4 MX95 SDPS: 0x1FC9 0x015D 0x0002 61F49AAB2DCB4DDF



C:\Users\nxa22585>C:\Users\nxa22585\Downloads\i.mx95\uuu.exe -b emmc_all C:\Users\nxa22585\Downloads\i.mx95\imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all C:\Users\nxa22585\Downloads\i.mx95\core-image-minimal-imx8mnevk.rootfs.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1

Success 1 Failure 0


1:2-61F49AAB 8/ 8 [Done ] FB: done
2:4-61F49AAB 3/ 3 [=================100%=================] SDPV: jump -scanlimited 0x800000


C:\Users\nxa22585>


Re: Falcon Mode Enablement - iMX8MP_EVKPlease help here i have stucked in this partRe: Falcon Mode Enablement - iMX8MP_EVK

In previous reply you gave a reference command for IMX95FRDM is that falcon enabled? 

Here you can find what i was done in Yocto - IMX8MP

1) meta-imx-fastboot - lf-6.12.20-2.0.0-secure - Github_Link
2) Added this meta to my source - Github_Link
3) And followed all the instruction gave by  AN14641 document.
4)Bitbake commands that i followed: 
bitbake -c clean linux-imx && bitbake -c clean imx-boot && bitbake -c clean u-boot-imx && bitbake -c clean imx-atf && bitbake -c clean imx-image-core 

bitbake -c compile linux-imx && bitbake -c compile imx-boot && bitbake -c compile u-boot-imx && bitbake -c compile imx-atf && bitbake -c compile imx-image-core


bitbake linux-imx && bitbake imx-boot && bitbake u-boot-imx && bitbake imx-atf && bitbake imx-image-core

5) 
CASE 1: sudo ./uuu -b emmc_all imx-image-core-imx8mpevk.rootfs-20260617095251.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-5-g124d086

Success 0 Failure 0


1:2-152E1000 1/ 1 [=================100%=================] SDPS: boot -scanterm -f /home/smurugan8/YOCTO/LWT/image/imx-image-core-imx8mpevk.rootfs-20260617095251.wic -scanlimited 0x800000



CASE 2: 

sudo ./uuu -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-core-imx8mpevk.rootfs-20260617095251.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-5-g124d086

Success 0 Failure 1


1:2-152E1000 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f imx-boot-imx8mpevk-sd.bin-flash_evk -scanlimited 0x800000


IMPORTANT : I NEED TO FLASH A FALCON ENABLED OS INTO eMMC 

Re: Falcon Mode Enablement - iMX8MP_EVK

Please note uuu is only used to program images to emmc, it doesn't check the content of your images.

I suspect there is problem with your uuu command itself.

Where did you download uuu?

Please download the latest UUU from https://github.com/nxp-imx/mfgtools/releases

Please download the Windows version UUU to do verification.

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi yipingwan

I also tried using the UUU tool on Windows, but I am seeing the same result—it still does not work for flashing eMMC.  I have attached the UUU -log.

However, when I flash the same Falcon-enabled OS to an SD card, it boots and works correctly. This confirms that the image itself and the Falcon configuration are valid.

My question is:

  • Why am I unable to flash this Falcon-enabled image to eMMC, even though the same image works from SD?
  • Is there any alternative or recommended method to flash a Falcon-enabled OS to eMMC, other than using UUU?

Could you please advise on the supported or reliable procedure for flashing eMMC in this scenario?Screenshot 2026-06-22 122141.png

Re: Falcon Mode Enablement - iMX8MP_EVKPlease help here.Re: Falcon Mode Enablement - iMX8MP_EVK

Please execute the following command with your Windows version UUU and send the result to me to do more investigation.

uuu.exe -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk   imx-image-core-imx8mpevk.rootfs-20260617095251.wic

Re: Falcon Mode Enablement - iMX8MP_EVK

Please try the following command

uuu.exe -b emmc_all  C:\Users\vvdn\Sanjiv\Falcon\imx-boot-imx8mpevk-sd.bin-flash_evk C:\Users\vvdn\Sanjiv\Falcon\imx-image-multimedia-imx8mpevk.rootfs-20260624074743.wic

Then send the result to me again.

Re: Falcon Mode Enablement - iMX8MP_EVK

Here you can find the output,

PS C:\Users\vvdn\Sanjiv\uuu_source-uuu_1.5.243\uuu-uuu_1.5.243\uuu> .\uuu.exe -b emmc_all C:\Users\vvdn\Sanjiv\Falcon\imx-boot-imx8mpevk-sd.bin-flash_evk C:\Users\vvdn\Sanjiv\Falcon\imx-image-multimedia-imx8mpevk.rootfs-20260624074743.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1

Success 0 Failure 1


1:3-152E1000 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f C:\Users\vvdn\Sanjiv\Falcon\imx-b...

Re: Falcon Mode Enablement - iMX8MP_EVK

Screenshot 2026-06-22 171137.png


I above you can find the log of UUU, 
Command=> .\uuu.exe -b emmc C:\Users\vvdn\Sanjiv\Falcon\imx-boot-imx8mpevk-sd.bin-flash_evk C:\Users\vvdn\Sanjiv\Falcon\imx-image-multimedia-imx8mpevk.rootfs-20260624074743.wic

But it is not working in eMMC , Same Image will work in SD Card

Re: Falcon Mode Enablement - iMX8MP_EVK

I verified on IMX8MP_EVK target board, there is no problem to program emmc, please refer to my following log.

C:\Users\nxa22585>C:\Users\nxa22585\Downloads\i.mx95\uuu.exe -b emmc_all C:\Users\nxa22585\Downloads\i.mx95\imx-boot-imx8mpevk-sd.bin-flash_evk C:\Users\nxa22585\Downloads\i.mx95\core-image-minimal-imx8mnevk.rootfs.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1

Success 1 Failure 0


2:4-0F0B9800 8/ 8 [Done ] FB: done


C:\Users\nxa22585>


Please extracted my image from the attached file, and only execute the following command.

uuu.exe -b emmc imx-boot-imx8mpevk-sd.bin-flash_evk

If it still fails, it seems there is problem with EMMC itself on your target board.

You could use the following emmc command to check whether you could write something to emmc in u-boot.

Usage:
mmc read addr blk# cnt
mmc write addr blk# cnt
mmc erase blk# cnt

Re: Falcon Mode Enablement - iMX8MP_EVK

Please only try whether you can write a default boot image to emmc with UUU.

Re: Falcon Mode Enablement - iMX8MP_EVKYes, @yipingwang,

When I include the meta-imx-fastboot layer in my build, the flashing process gets stuck. However, if I remove the meta-imx-fastboot layer, I am able to flash the image to eMMC successfully.
Re: Falcon Mode Enablement - iMX8MP_EVKI have one question @yipingwang it is falcon enabled imageRe: Falcon Mode Enablement - iMX8MP_EVKPlease help here.. @yipingwangRe: Falcon Mode Enablement - iMX8MP_EVK

Please send /home/smurugan8/YOCTO/LWT/image/falcon_mode/imx-boot-imx8mpevk-sd.bin-flash_evk to me.

I will do verification on my target board.

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi @Sanjiv_Mns 

The meta-secure-boot Yocto layer is not implemented for the 6.12.20 BSP. Since the meta-imx-fastboot layer depends on the meta-secure-boot, the branch lf-6.12.20-2.0.0-secure does not implement secure boot.

The 0001-imx8m-reset-ethernet-phy-in-spl.patch patch is mandatory if you need to use the Ethernet interfaces in Linux. It resets the PHYs, without which the Linux driver cannot initialize the interfaces.

Re: Falcon Mode Enablement - iMX8MP_EVK

Please find the attachment .

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi @yipingwang ,
I have done the commands which you gave in previous reply, here you can find the command logs & Boot logs

COMMAND LOGS:
sudo ./uuu -b emmc_all /home/smurugan8/YOCTO/LWT/image/default/imx-boot-imx8mpevk-sd.bin-flash_evk /home/smurugan8/YOCTO/LWT/image/default/imx-image-multimedia-imx8mpevk.rootfs-20260622071640.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-5-g124d086

Success 1 Failure 0

1:1-152E1000 8/ 8 [Done ] FB: done

sudo ./uuu -b emmc /home/smurugan8/YOCTO/LWT/image/default/imx-boot-imx8mpevk-sd.bin-flash_evk /home/smurugan8/YOCTO/LWT/image/falcon_mode/imx-boot-imx8mpevk-sd.bin-flash_evk
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-5-g124d086

Success 1 Failure 0
1:1-152E1000 7/ 7 [Done ] FB: Done

BOOT LOGS:
U-Boot SPL 2025.04-g44898b9f3cfe-dirty (Sep 03 2025 - 09:56:50 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC2
spl_load_image_fat: error reading image kernel-atf-dtb.itb, err - -5
spl_load_image_fat: error reading image u-boot-atf.itb, err - -5
Error: -2
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi @Sanjiv_Mns 

Falcon Mode images works on both SD and eMMC. To flash a Falcon image on eMMC/SD you need to:

1. Build the default bootloader. In a clean Yocto environment, run: bitbake imx-boot. Make sure the meta-imx-fastboot layer is not added at this step.

This will generate the tmp/deploy/images/imx8mp-lpddr4-evk/imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk default bootloader.

2. Build the falcon mode bootloader and the falcon mode image. Add the meta-imx-fastboot layer to your BBLAYERS.

  • To compile the falcon mode bootloader, run:

bitbake imx-boot

This command will generate the tmp/deploy/images/imx8mp-lpddr4-evk/imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk_dual_bootloader falcon bootloader. This bootloader contains only the SPL, without the U-Boot proper. When the meta-imx-fastboot layer is added, the *_dual_bootloader is generated. See layer.conf.  

  • To compile the falcon mode image, run:

bitbake imx-image-multimedia

This will generate the tmp/deploy/images/imx8mp-lpddr4-evk/imx-image-multimedia-imx8mp-lpddr4-evk.rootfs.wic.zst image.

3. Use UUU to flash the image on the eMMC. UUU is the only tool available to flash images on the eMMC.

uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mp-lpddr4-evk.rootfs.wic.zst

uuu -b emmc imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk_dual_bootloader

Re: Falcon Mode Enablement - iMX8MP_EVK

Please remove bld-xwayland build folder to rebuild images.

$ rm -rf bld-xwayland
$ MACHINE=imx8mpevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland
$ bitbake-layers add-layer ../sources/meta-imx-fastboot

Please add the following line in bld-xwayland/conf/local.conf

FALCON_KERNEL_BOOTARGS:mx8mp-generic-bsp = "console=ttymxc1,115200 root=/dev/mmcblk2p2 rootwait rw quiet"

Then rebuild images:

$ bitbake imx-boot
$ bitbake core-image-minimal

uuu.exe -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk core-image-minimal-imx8mpevk.rootfs.wic

uuu.exe -b emmc imx-boot-imx8mpevk-sd.bin-flash_evk imx-boot-imx8mpevk-sd.bin-flash_evk_falcon

Please refer to my verification log:

U-Boot SPL 2025.04-g9383f8387dc7-dirty (Jun 04 2025 - 09:48:20 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC2
Failed to find node!, err: -11!
Failed to find node!, err: -11!
NOTICE: Do not release JR0 to NS as it can be used by HAB
NOTICE: BL31: v2.12.0(release):lf-6.12.20-2.0.0-dirty
NOTICE: BL31: Built : 08:15:07, May 9 2025
[ 0.324123] imx8mp-ldb ldb-display-controller: Failed to create device link (0x180) with 32e90000.lcd-controller
[ 0.395104] : mipi_csis_imx8mp_phy_reset, No remote pad found!
[ 0.514210] imx8mp-ldb ldb-display-controller: Failed to create device link (0x180) with 1-004c
[ 0.576883] imx8mp-ldb ldb-display-controller: Failed to create device link (0x180) with 1-004c
[ 0.625848] ov5640 1-003c: ov5640_write_reg: error: reg=3008, val=42
[ 0.632862] ov5640 1-003c: ov5640_write_reg: error: reg=3103, val=11
[ 0.639669] ov5640 1-003c: ov5640_read_reg: error: reg=3108
[ 0.645268] ov5640 1-003c: failed to power on
[ 0.661389] imx8mp-ldb ldb-display-controller: Failed to create device link (0x180) with phy-lvds
[ 0.694937] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e60000 to encoder DSI-41: -19
[ 0.706570] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[ 0.714859] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -19

NXP i.MX Release Distro 6.12-walnascar imx8mpevk ttymxc1

imx8mpevk login: root
root@imx8mpevk:~#


Re: Falcon Mode Enablement - iMX8MP_EVK

Please use the following commands to program images to the target board with UUU.

unzstd <image_name>-[secure-boot]-<machine_name>.rootfs.wic.zst
uuu -b emmc_all <default_bootloader> <image_name>-<machine_name>.rootfs.wic
uuu -b emmc <default_bootloader> <falcon_mode_bootloader>

 The first parameter is the default bootloader, falcon mode bootloader is only specified in the second parameter of the second uuu command.

Re: Falcon Mode Enablement - iMX8MP_EVK

Hi @yipingwang & @elena_popa 
Thank you so much for your support

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-28-2026 02:26 AM
更新者: