2380551_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2380551_en-US

2380551_en-US

LS2088ARDB: How to recover when QSPI Flash is corrupted

Hi

I was able to boot LS2088ARDB in QSPI-Boot mode. The QSPI-FLash has some preflashed boot images (bl2_qspi.pbl, RCW, fip.bin).

Accidentally I erased the boot images in QSPI-FLash. Now the board does not boot in QSPI-Boot mode.

I used Lauterbach JTAG - Trace32 and used the script `present at the path  C:\T32\demo\arm\hardware\ls208x\ls2088a\ls2088a-rdb\ls2088a_sieve_sram_failsave.cmm

The script does the below

1)override RCW_src=Hardcoded,

2)JTAG Uses the basic RCW present int he script and boots

3)Loads basic app into internal RAM


Question: 

1) Can you provide us with a script which will configure clocks and DDR so that we can load U-boot onto RAM.

2) Also please provide steps OR correct me if my recovery steps are not proper.

3) Also in the path C:\T32\demo\arm\flash we dont see flash script for ls2088ardb. Can you please provide if you have it.


Thanks and Regards

Re: LS2088ARDB: How to recover when QSPI Flash is corrupted

NXP only provides CodeWarrior to the customer.

You could refer to section "9.4 Board recovery in case of missing/corrupt RCW in IFC memory" in the attached CodeWarrior document.

Please refer to the attached CodeWarrior initialization file for LS2088ARDB.

Tags (1)
No ratings
Version history
Last update:
‎06-16-2026 02:36 AM
Updated by: