I have installed the S32 Design Studio on my ubuntu 22.0 linux system, but i am not able to see the Real time drivers package in Extensions and Updates tab even after added the update sites for the RTD package. Also when i opened it today it automatically checked for the updates and given this error you can see in the image:
varunpenumudi_0-1781236748272.png
The error says this:
"Cannot complete the install because one or more required items could not be found.
Software being installed: Remote Services 12.5.0.202603111352 (org.eclipse.remote.feature.group 12.5.0.202603111352)
Missing requirement: Eclipse Remote Development documentation plug-in 12.5.0.202603111352 (org.eclipse.remote.doc.isv 12.5.0.202603111352) requires 'osgi.bundle; org.eclipse.help [3.10.500,4.0.0)' but it could not be found
Cannot satisfy dependency:
From: Remote Services 12.5.0.202603111352 (org.eclipse.remote.feature.group 12.5.0.202603111352)
To: org.eclipse.equinox.p2.iu; org.eclipse.remote.doc.isv [12.5.0.202603111352,12.5.0.202603111352]
"
please help me with solving this issue
Hi,
unfortunately RTD is not supported on Linux OS. It can be installed from a .zip archive, but it is not tested and there are couple known limitations caused by case sensitive OS (Linux).