2380505_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2380505_en-US

2380505_en-US

Issue with the FS32K144UAVLL crystal oscillator!

Manager:

We are using the FS32K144UAVLL with a 20 MHz crystal oscillator, a 10 pF matching capacitor, and a 1 MΩ load resistor. The crystal oscillator outputs a single-ended 20 MHz sine wave to ground with a 0.5 Vp-p amplitude. The MCU cannot run the program when using the external crystal oscillator, but it works fine when using the internal crystal oscillator.

Using the development board software, the FS32K144HFVL development board, with an 8 MHz crystal oscillator, a 22 pF coupling capacitor, and a 1 MΩ load resistor; the crystal oscillator outputs a single-ended 8 MHz sine wave with a peak-to-peak voltage of 1 V.

May I ask:

1. What is the difference between the FS32K144UAVLL and the FS32K144HFVL? Can the same program be used for both? Do they require the same external crystal oscillator?

2. What is the acceptable amplitude for the external crystal oscillator of the FS32K144UAVLL?

3. How do I adjust the amplitude of an external crystal oscillator?

Thank you!

回复: FS32K144UAVLL晶振问题!

Hi @YF666666 

In Section 4 of the S32K1xx Data Sheet, it is noted that a core frequency of 112 MHz is not supported for the M temperature range (–40°C to 125°C).

I recommend referring to the S32K1xx_Orderable_Part_Number_List.xlsx, which is attached to the data sheet, to verify the available part numbers and identify the options that meet your requirements.

Re: FS32K144UAVLL晶振问题!

Hi @YF666666 

1. Device Differences

FS32K144UAVLL

  • U: Core frequency up to 112 MHz
  • A: Includes CAN FD, FlexIO, and Security features

FS32K144HFVLL

  • H: Core frequency up to 80 MHz
  • F: Includes CAN FD and FlexIO (no security features)

2. The S32K1xx family supports external crystals or resonators in the range of 4 MHz to 40 MHz.

3. You may find the following documents helpful for crystal oscillator design and amplitude considerations:

  • AN14518: Crystal Oscillator Design Guide
  • AN5426: Hardware Design Guidelines for S32K1xx

These references provide detailed guidance on oscillator configuration, load capacitors, and design best practices.


BR, VaneB

回复: FS32K144UAVLL晶振问题!

Manager:

Does the FS32K144UAT0VLLT have a clock speed of 112 MHz and an operating temperature range of -40°C to +105°C?

We use it in automobiles, which require an automotive-grade temperature range of -40° to +125°,

The chip model has been changed to FS32K144UAT0MLLT, with a clock speed of 112 MHz and an LQFP100 package. Is this the correct model?

If the model number is incorrect, please send us the correct one. Thank you!

Re: FS32K144UAVLL晶振问题!

You may try FS32K144UAVLL with an 8 MHz crystal oscillator, a 22 pF coupling capacitor, and a 1 MΩ load resistor

Tags (1)
No ratings
Version history
Last update:
‎07-01-2026 03:30 AM
Updated by: