2380305_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2380305_en-US

2380305_en-US

Flutter on IMX93

Hello
I have an IMX93 board and I'm trying to run a flutter program on it. I'm having a loto of trouble with CPU usage (around 20% for a static screen with a clock that refresh every second, and over 90% for a full page scroll with images). Most of it depends from raster (around 180ms each second in the static screen). I am trying to enable PxP but either I am not able to either flutter can not use it to rasterize.

I saw that flutter uses OpenGl ES, Vulkan and metal as API, so I'm not sure if it is possible to use pxp to help CPU. 

Thanks

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-12-2026 03:29 AM
更新者: