Hello,
I'm currently working with S32K314 microcontroller, using S32K344_0_2_55_0 HSE with AB swap configuration.
I'm trying to import a AES CMAC key using service HSE_SRV_ID_IMPORT_KEY and it always return HSE_SRV_RSP_INVALID_PARAM. My current microcontroller state is:
- Lifecycle = CUST_DEL (0x04)
- INSTALL_OK = 0
I've try to create a custom AES catalogue. This request generates an error error HSE_SRV_RSP_NOT_ALLOWED 0xAA55A21.
I've make sure that all the buffers that parsed to HSE are located inside SRAM.
I even manage to run the erase service. It respond ok.
Given all the above I sill end up in HSE_SRV_RSP_INVALID_PARAM error.
Any idea what I could check next?
Thank you in advance!
Hello @lukaszadrapa .
Thank you for the quick response.
I've tried to installed the key catalogue with a minimal configuration, but it was not successful. It respond with HSE_SRV_RSP_NOT_ALLOWED.
This is my catalogue configuration.
CosminSbera_0-1781250627017.png
Any tips on what I could check next?
Thank you in advance!
Hi @CosminSbera
If HSE_STATUS_INSTALL_OK is ‘0’, the catalogs are not formatted, so you can’t import a key.
How did you configured the catalogs?
Take a look at description of hseFormatKeyCatalogsSrv_t structure in HSE Service API reference manual:
c:\NXP\HSE_FW_S32K344_0_2_55_0\docs\S32K3X4_HSE_Service_API_Reference_Manual.pdf
There’s a list of requirements which need to be met.
And take a look at section “6.1.5.3 Key catalog formatting” in HSE firmware reference manual rev. 2.7. There’s a list of reasons why the formatting may fail.
Regards,
Lukas
All groups in RAM catalog must use owner HSE_KEY_OWNER_ANY. You can’t use HSE_KEY_OWNER_CUST here.
All groups in NVM catalog must use owner HSE_KEY_OWNER_CUST or HSE_KEY_OWNER_OEM. But HSE_KEY_TYPE_SHE is an exception – this must be HSE_KEY_OWNER_ANY also in NVM catalog.
lukaszadrapa_0-1781266224583.png
lukaszadrapa_1-1781266231149.png
Regards,
Lukas