Hello.
I am interfacing ultrasonic sensor to MIMX RT1170 EVK board. For interfacing the sensor I need to use Arduino interface for GPIOs connection. I am not able to find the proper connections for ultrasonic sensor connection, because not getting power at the pins.
I gave supply to board using adapter (J43).
I need reference for pins connection and are there any settings required for powering ON the arduino interface region?
Thank you.
Hi @SK02 ,
Thank you so much for your interest in our products and for using our community.
regarding your issue, could you please verify the following power configuration?
1: The adapter is connected to J43
2: The SW5 power switch is turned ON
3: J38 is set to pins 1–2 to select the external 5 V input
Once these settings are confirmed, the board power rails—including those supplying the Arduino interface—should be available.
Please try it.
Best Regards
May