2379781_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2379781_en-US

2379781_en-US

Does the S32K364 support partial AB_SWAP mode?

Hello! I have a customer’s S32K364 board here, which already has HSE configured in AB_SWAP mode. When I read the value of the DCMSTAT (0x402AC000) register, it is 0x00040FF1. According to the manual, this indicates that the DCMOTAA_EX bit is set.and the chip is in partial AB_SWAP mode. However, the manual also states, “This AB_SWAP mode is supported only for S32K328, S32K338, S32K348, S32K358, S32K356, S32K336, and S32K388." Is this a documentation error or is there another reason for this?

Re: Does the S32K364 support the partial AB_SWAP mode?

Hi@BianHaopeng1

看错文档了你,RN00176-for S32K396 HSE Firmware 0.2.50.0。

Senlent_0-1781161383580.pngSenlent_0-1781161383580.png


Re: Does the S32K364 support the partial AB_SWAP mode?

For the S32K394, S32K374, and S32K364 devices, 0040_0000h is not available for IVT during AB-SWAP for boot loader but the ABSWAP function should be common feature

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-12-2026 03:30 AM
更新者: