2377353_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2377353_en-US

2377353_en-US

AVB Import Error

Tony_Tan_7-1780649389754.png


 

Hi, importing TRESOS project from SW32K5_AVB_M7_0.8.0_CD02_D2606 reported more than 5000 errors, what is the reason and how to solve it. Thanks!


 
 

 

回复: AVB 导入报错

Hi Tony.

Sorry for the inconvenience.

After I installed SW32K5_RTD_R23-11_0.8.1_CD03_D2604.exe and SW32K5_AVB_M7_0.8.0_CD02_D2606.exe, importing a project using tresos Studio 32.0 still reports errors.

Although AVB_S32K5_AVTP_IntegrationManual.pdf mentions S32K5 RTD Drivers 0.8.1 CD03, I see in EB Tresos' Module Configurations Dio\Port SW.Version: 0.8.1 D2605. This looks more like the version of SW32K5_RTD_R23-11_0.8.1_D2605.exe you downloaded earlier.

Please wait for a response from the internal team and then use the EB Tresos Studio 32.1.4 import to verify if the EB version is causing this.

Best Regards,
Robin

回复: AVB 导入报错

Hi Robin.

Thank you for your response and look forward to hearing back from your internal team.


回复: AVB 导入报错

1. EB Tresos 32.1.4 is now available for download and installation:
Please click on S32K3 Standard Software - > Automotive SW - EB tresos Studio / AUTOSAR Configuration Tool - > EB tresos Studio 32.1.4

2. I uninstalled the previously installed SW32K5_AVB_M7_0.8.0_CD02_D2606, SW32K5_M7_gPTP_0.8.0_D2605, SW32K5_RTD_R23-11_0.8.1.

3. Reinstall SW32K5_RTD_R23-11_0.8.1_D2605.exe, SW32K5_M7_gPTP_0.8.0_D2605.exe, SW32K5_AVB_M7_0.8.0_CD02_D2606.exe and select the latest installation for EB Tresos install directory. directory to the latest installation of EB Tresos 32.1.4. Path.

4. Import the AVB project in SW32K5_AVB_M7_0.8.0_CD02_D2606, now you can generate code normally!

SW32K5_AVB_M7_0.8.0_CD02_D2606 Generate code.png

回复: AVB 导入报错Thanks, it works now.
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-16-2026 03:29 AM
更新者: