2377059_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2377059_en-US

2377059_en-US

MCXE247 Error with Config Tools in McuXpresso

I imported the simple led_blinky example in the Eclipse based McuXpresso IDE (v24.12).

Though it builds and debugs, I cannot open the config tools. I receive the error "Processor MCXE247 is not supported or data for the processor is not available. Check the Internet connection" I am using SDK 26.03.00 with the FRDM MCX E247 board.

I also imported an example for the MCXA153. I can access the Config Tools for that project without any problems.

Is the MCX E series supported by Config Tools?

Also, is Config Tolls integrated into the mcuXpresso for VSCode, or do I need to use the standalone Config executable?


Package and IO|GPIORe: MCXE247 Error with Config Tools in McuXpresso

Hello @hns80 

Thanks for your sharing. Your answers are correct.

Regarding your new question, do you mean VS Code or MCUXpresso IDE? Please provide a video or screenshots showing your steps, and I will help check on my side. Thank you.

BR

Alice

Re: MCXE247 Error with Config Tools in McuXpresso

Answering my own questions:

1. I was getting the error about an unsupported device because I was running version 24.12. 
   After updating to version 25.6, it works

2. The configurator is included in vscode if it is installed in the McuXpresso installer. When creating a new project, there is a checkbox to use it.  It timed out on me when I tried to enable it, but it seems to at least try.


I wonder if it's possible to add the configurator to an existing project? With the examples I imported, when I right click on the project and select Open with McuXpresso Config Tools, I get a message stating "Cannot find and configuration files"



タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-05-2026 03:31 AM
更新者: