2376361_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2376361_en-US

2376361_en-US

Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289

I am considering purchasing either the FRDM-A-S32K358 or the S32K3X8EVB-Q289 model. However, what are the hardware differences between the S32K3X8EVB-Q289 and the FRDM-A-S32K358?

I was told in a previous question that the SD card function is implemented on the FRDM-A-S32K358. I want to know if the other pins or features like CAN communication are present on the board. I want to know if they are implemented exactly the same way as the S32K3X8EVB-Q289. I would also like to know if there are any software differences. Or is there a separate circuit diagram? It would be easier for me to make a decision based on that.

Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289

You are currently using a gmail account and the company information is not visible in the system. Please also provide me with the NDA number separately so I can have a colleague check if the NDA is still valid.

Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289

Our company has an NDA in place. It seems likely that this is possible, but can you confirm if they will process it immediately if I request it via a support ticket?

Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289

Hi

Since this FRDM-A-S32K358 has not yet been officially released, the schematics or hardware manuals are not available for download at this time.

Could you please provide your project and company information separately? Have you signed an NDA? This would allow me to contact internal team to obtain information about the development board in advance.

Currently, I can tell you that the FRDM-A-S32K358 has a CAN interface:
This board integrates NXP’s TJA1043 CAN transceiver, with its output routed to connector J15.
CAN0_RX PTA6
CAN0_TX PTA7


I can only see the initial version of the UM12541 FRDM-A-S32K358 development board internally at this time. I've attached the document's bookmarks to give you a general overview of its features. However, more detailed information will likely require you to sign an NDA or wait for the official release of the FRDM.

bookmark UM12541 FRDM-A-S32K358 development board.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-05-2026 03:30 AM
更新者: