2375452_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2375452_en-US

2375452_en-US

U4N: How to Skip the Hardest Grind in FH6

Forza Horizon 6 is finally here, and Playground Games has delivered what fans have been begging for years: a massive, gorgeous, neon-soaked recreation of Japan. From drifting down the Kawazu-Nanadaru Loop to tearing through the ultra-dense streets of Tokyo City, the map is a car enthusiast’s dream.

But there’s a catch. This year, the developers didn’t just copy-paste the sandbox progression from the previous games. They reintroduced a strict, old-school progression structure. You don't start as the superstar festival boss anymore; you start as a literal tourist. To unlock the endgame areas like Legend Island or get behind the wheel of S2-class hypercars, you have to grind your way through qualifying events and earn successive Wristbands.

For purists, it’s a welcome challenge. For the rest of us who just want to customize a 1997 Nissan Silvia, tune it to perfection, and cruise with friends at a Car Meet, the progression is an absolute wall.

Here is exactly how the math breaks down on the hardest grind in Forza Horizon 6, and how players are choosing to bypass it.

The Cold Hard Math of the Horizon Grind

To understand why players are looking for alternatives, you just have to look at the numbers. Forza Horizon 6 boasts a massive roster of over 550 real-world cars at launch. Want a garage full of legendary JDM icons and high-end exotics? You’ll need tens of millions of Credits (CR).

Playground Games has tucked 200 hidden mascots across Japan, each giving you 5,000 CR when you smash them. If you manage to find every single one, that’s a clean 1,000,000 CR. Sounds great, right? Except a single top-tier car like the Ferrari J50 can easily wipe out that entire balance in one click.

Then there’s the time investment:

  • The Average Race: Yields roughly 10,000 to 15,000 CR depending on your difficulty multipliers and assists.

  • The Math: To buy a high-end 2,000,000 CR hypercar, you need to complete roughly 130 to 200 races.

  • The Time: At an average of 4 minutes per race (including load screens and menus), that is 9 to 13 hours of continuous, repetitive racing just for one car.

And that doesn't even account for the cost of performance parts, cosmetic body kits, or buying premium player houses like the Valley Estate to showcase your collection. If you have a full-time job or school, turning Forza into a second shifting job just to experience the best parts of the game isn't appealing.

Skipping the Bottleneck

Because of this steep curve, a huge portion of the community is choosing to buy their way past the tedious introductory phases. Instead of spending 50 hours sitting in slow C-class hatchbacks waiting for the game to "let them have fun," players are using third-party services to get established instantly.

If you want to jump straight into late-game Touge battles or fully build out custom tracks in the new multiplayer CoLab tool without worrying about your budget, relying on trusted platforms is the most straightforward shortcut. For example, safe marketplaces like U4N allow players to bypass the economy grind entirely; you can easily buy forza horizon 6 mods or loaded accounts to instantly unlock the 550+ car roster, stack up hundreds of millions of credits, and get maximum wristbands without the repetitive headaches.

A Note on Safety: If you do decide to skip the grind, always use reputable platforms that use safe delivery methods to protect your Xbox or Steam account from standard automated anti-cheat flags.

Should You Skip It?

Whether you should take the shortcut depends entirely on what kind of player you are:

  • The Progression Lover: If you genuinely enjoy starting from zero, hunting down all 14 Barn Finds, searching for the 9 hidden treasure cars, and slowly earning your way to the top of the Horizon Invitational, take your time. The campaign is well-crafted.

  • The Sandbox Customizer: If your main joy comes from tuning, livery design, drifting down Mount Fuji with your crew, and testing the limits of the physics engine in custom EventLab maps, the wristband progression system is just a time-gate keeping you from the game you actually paid for.

Forza Horizon 6 is arguably the best racing game of the generation, but it demands an enormous amount of your free time. Knowing how the economy functions allows you to decide whether you want to earn every single credit manually, or take a quick lane change straight to the endgame.

タグ(1)
評価なし
バージョン履歴
最終更新日:
昨日
更新者: