2372705_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2372705_en-US

2372705_en-US

PN5190 Offscreen NFC Test PCD Analog TA132 4-plane FAIL

Hello, we are developing an off-screen NFC, and we are currently experiencing some problems with the PCD Analog test: TA132's 4-plane test Fail

mark_tang_0-1780020039933.png

mark_tang_1-1780020407051.png


The contents of the FAIL are shown in the figure, and so far it has been verified as follows:

1. Extinguish the screen to test PASS

2. When lighting up the screen, the maximum output voltage of DPC needs to drop to 4.5V, TA132 4-plane test PASS, but TAB111 4-plane field voltage will Fail!

3. In the middle of the attempt to debug the ARC parameters, the test results did not significantly improve the effect, please ask whether there are other parameters can be optimized

4. Read 5190 documentation, mentioned SDT can solve this problem, please advise how to correctly debugging

mark_tang_2-1780020479057.png

We have tried debugging, with TypeA parameters loaded, no specific waveform information (GTK wave) in the captured log, using the recommended Signal Detection Threshold, no improvement

mark_tang_3-1780020766610.png

mark_tang_4-1780020849062.pngmark_tang_5-1780020868797.png






Re: PN5190 屏下NFC测试PCD Analog TA132 4平面failTested with loopback, also tested with transaction send A, both reported errors.Re: PN5190 屏下NFC测试PCD Analog TA132 4平面fail

Hello @mark_tang 

Please use EMVCo stack to test as the below:

KaiLi_0-1780293471461.png


Re: PN5190 屏下NFC测试PCD Analog TA132 4平面fail

Hello @mark_tang

Was the antenna under the screen when you tested it?

Re: PN5190 屏下NFC测试PCD Analog TA132 4平面fail

Yes, the antenna has three edges under the screen glass and one edge directly below the screen (the metal frame behind the screen has been removed), schematically as follows

mark_tang_0-1780446827314.png


Re: PN5190 屏下NFC测试PCD Analog TA132 4平面failHello, any suggestions, this side of the debugging passive matching has not much progress, TA132's 4-plane test Fail this problem has not been solved!
タグ(1)
評価なし
バージョン履歴
最終更新日:
3 週間前
更新者: