LPC804M101(Jなし)の温度範囲を知りたいのですが、データシートにはLPC804M101JDH20(温度範囲-10~+105)しか記載されておらず、私が持っている製品にはJの文字の刻印がありません。写真を2枚添付しました。
LPC804M101デバイスは、「J」接尾辞に関わらず、–40°Cから+105°Cの同じインダストリアル動作温度範囲を共有しています。接尾辞は主にパッケージの種類を示しており、グレードの違いはないので、Jマークされていない部品はその全範囲で有効であるはずです。認証やコンプライアンスの目的では、NXPの公式データシートやサポートで確認するのが最善ですが、実際には-40°Cから+105°Cの範囲で信頼できます。