2372472_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2372472_en-US

2372472_en-US

Not found on datasheet marking without "J" of LPC804M101JDH20

I need to know temperature range for LPC804M101 (without J), datasheet only shows LPC804M101JDH20 (temperature range -10 to + 105) and I have a piece and no letter J marking.  I attached 2 pictures. 

Re: Not found on datasheet marking without "J" of LPC804M101JDH20

The LPC804M101 devices, regardless of the “J” suffix, share the same industrial operating temperature range of –40 °C to +105 °C. The suffix mainly indicates package type rather than a different grade, so your non‑J marked part should still be valid for that full range. For certification or compliance purposes, it’s best to confirm with NXP’s official datasheet or support, but practically you can rely on –40 °C to +105 °C.

 
Tags (1)
No ratings
Version history
Last update:
2 weeks ago
Updated by: