Hi,
I'm working with the Variscite SOM VAR-SOM-MX8M-PLUS (you can find their website when googling this SOM model) that is using LVDS for a 640x480 60Hz LCD. I'm unable to get a stable image for the LCD when using the display timing parameters from the spec sheet.
My device tree changes:
#include "imx8mp-var-som-symphony.dts" / { panel { compatible = "panel-lvds"; backlight = <&backlight>; width-mm = <211>; height-mm = <158>; label = "640x480"; data-mapping = "jeida-24"; status = "okay"; panel-timing { clock-frequency = <25175000>; hactive = <640>; vactive = <480>; hback-porch = <40>; hfront-porch = <8>; vback-porch = <25>; vfront-porch = <2>; hsync-len = <96>; vsync-len = <2>; hsync-active = <0>; vsync-active = <0>; de-active = <1>; }; port { panel_in: endpoint { remote-endpoint = <&lvds_out>; }; }; }; }; &clk { assigned-clock-rates = <0>, <0>, <1000000000>, <800000000>, <500000000>, <400000000>, <800000000>, <393216000>, <361267200>, <352450000>; }; &media_blk_ctrl { assigned-clock-rates = <500000000>, <200000000>, <0>, <0>, <352450000>; }; &ldb { status = "okay"; lvds-channel@0 { fsl,data-mapping = "jeida"; fsl,data-width = <24>; status = "okay"; port@1 { reg = <1>; lvds_out: endpoint { remote-endpoint = <&panel_in>; }; }; }; };
I've updated the PLL clocks to reflect the 25.175 MHz pixel clock (25.175 * 14 = 352.450MHz) I've also added other clocks incase there was different multiplier (not just 14).
static const struct imx_pll14xx_rate_table imx_pll1443x_tbl[] = { PLL_1443X_RATE(1039500000U, 173, 2, 1, 16384), /* 74.25 MHz */ PLL_1443X_RATE(910000000U, 455, 3, 2, 0), /* 65 MHz */ PLL_1443X_RATE(1040000000U, 208, 3, 1, 0), /* 65 MHz */ PLL_1443X_RATE(455000000U, 379, 5, 2, 10923), /* 65 MHz */ PLL_1443X_RATE(650000000U, 325, 3, 2, 0), PLL_1443X_RATE(594000000U, 198, 2, 2, 0), PLL_1443X_RATE(519750000U, 173, 2, 2, 16384), /* 37.125 MHz */ /*PLL_1443X_RATE(420000000U, 175, 5, 1, 0),*/ /* 30 MHz */ PLL_1443X_RATE(393216000U, 262, 2, 3, 9437), /*PLL_1443X_RATE(378000000U, 126, 4, 1, 0),*/ /* 27 MHz */ PLL_1443X_RATE(361267200U, 361, 3, 3, 17511), PLL_1443X_RATE(352450000U, 220, 15, 0, 18432), /* 25.175 MHz */ PLL_1443X_RATE(400000000U, 200, 3, 2, 0), /* 25 MHz */ PLL_1443X_RATE(700000000U, 175, 3, 1, 0), /* 25 MHz */ PLL_1443X_RATE(350000000U, 175, 6, 1, 0), /* 25 MHz */ PLL_1443X_RATE(245760000U, 328, 4, 3, 0xae15), PLL_1443X_RATE(225792000U, 226, 3, 3, 0xcac1), PLL_1443X_RATE(122880000U, 328, 4, 4, 0xae15), PLL_1443X_RATE(112896000U, 226, 3, 4, 0xcac1), PLL_1443X_RATE(61440000U, 328, 4, 5, 0xae15), PLL_1443X_RATE(56448000U, 226, 3, 5, 0xcac1), PLL_1443X_RATE(49152000U, 393, 3, 6, 0x374c), PLL_1443X_RATE(45158400U, 241, 2, 6, 0xd845), PLL_1443X_RATE(40960000U, 109, 1, 6, 0x3a07), };
I've commented out the hardcoded clocks inside imx8mp-ldb.c
/* * Due to limited video PLL frequency points on i.MX8mp, * we do mode fixup here in case any mode is unsupported. */ /*if (ldb->dual) mode->clock = mode->clock > 100000 ? 148500 : 74250; else mode->clock = 74250;*/ return 0;
Verified PLL clock on board:
root@imx8mp-var-dart:~# cat /sys/kernel/debug/clk/video_pll1/clk_rate
352450000
The picture looks like this
Please advise on what to try next.
Thanks,
Jon
refer to your panel spec, it seems you don't set correct timings, the h_total is 800 and v_total is 525, pls double check it
Bumping to be seen by support @joanxie