In this post, I want to share a quick walkthrough of Smart Device Gateway, a FastAPI-based demo server that allows connected devices to use local GenAI capabilities accelerated by the Ara240 DNPU.
The idea behind this demo is to centralize AI intelligence in one gateway instead of adding powerful AI hardware to every device. A connected device only needs a microphone, speaker, and network connection to become a voice-enabled assistant.
Smart Device Gateway enables devices such as appliances or embedded clients to send audio to a local server, process the request using speech recognition, RAG, an LLM running on Ara240 DNPU, and text-to-speech, then stream the spoken response back to the client.
The current demo showcases intelligent device assistants for a generic oven and coffee machine/barista use case, using device manuals as the knowledge base for contextual responses.
The Smart Device Gateway receives audio from a client over WebSocket, converts speech to text, retrieves relevant context from a device knowledge base, sends the prompt to the LLM through the eIQ AAF Connector, converts the generated response back to speech, and streams the audio response to the client.
At a high level, the flow is:
Audio Input → STT → RAG → eIQ AAF Connector / LLM → TTS → Audio Output
The LLM runs on the Ara240 DNPU, while the server runs on the FRDM i.MX platform.
Start the server:
run_server_only --host 0.0.0.0 --port 8080
The server expects the eIQ AAF Connector to already be running on 0.0.0.0:8000 with Qwen2.5-7B-Instruct properly configured.
Alternatively, the demo can start the server together with the connector:
run_server --host 0.0.0.0 --port 8080
The demo includes a push_to_talk client that can run on a host PC. After copying the push_to_talk folder, run:
python -m uv run push_to_talk.py --server_ip --port --device oven
You can also use:
python -m uv run push_to_talk.py --server_ip --port --device barista
If no device name is provided, the RAG knowledge base is not used and the response is generated from the LLM’s general knowledge.
In the attached video, I show how to start the Smart Device Gateway server, connect a client, select a device profile such as oven or barista, ask a voice question, and receive a spoken response generated locally using Ara240 DNPU acceleration.
Smart Device Gateway demonstrates how everyday devices can become voice-enabled assistants by connecting to a local AI gateway. By combining STT, RAG, LLM inference on Ara240 DNPU, and TTS, the demo provides a practical reference for building local, privacy-focused GenAI experiences on NXP i.MX platforms.