2371544_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2371544_en-US

2371544_en-US

EIQ Connector

eIQ AAF Connector


In this post, I want to share a quick walkthrough of eIQ AAF Connector, a REST-based server that enables LLM and VLM inference on NXP i.MX platforms using the Ara240 DNPU.

The connector provides a simple HTTP interface for client applications to send prompts and receive streaming token responses from models running locally on Ara240. It is also the communication layer used by applications such as LLM Edge Studio and VLM Edge Studio.

 

Key Features

  • REST API server for Ara240-accelerated model inference
  • Chat Completions-style HTTP endpoint
  • Streaming token responses
  • Support for text LLMs and Qwen2.5-VL models
  • Model configuration through server_config.json
  • Optional tool calling and guided generation support for compatible text models
  • Optional semantic prompt caching for text models
  • OpenAPI documentation available through the /docs endpoint

 

How It Works


The eIQ AAF Connector runs on the i.MX host and exposes a REST API. Client applications send prompts to the connector, which communicates with the Ara240 Runtime SDK and the loaded model.dvm running on the Ara240 DNPU. The response is returned as generated tokens, with support for streaming output.

 

Basic Setup


After installing the Debian package, activate the connector virtual environment:

source /usr/share/eiq/aaf-connector/venv/bin/activate

Run the connector:

connector

By default, the server starts on:

127.0.0.1:8000

To allow access from another device, start it with:

connector --host 0.0.0.0

 

Configuration


The connector uses a JSON configuration file named server_config.json to define server settings and available models. This includes model paths, tokenizer paths, model type, prompt size, tool calling support, and whether the model should be loaded at startup.

{
  "log_level": "INFO",
  "model_config_path": "/usr/share/llm/{}/",
  "model_tokenizer_path": "/usr/share/llm/{}/tokenizer",
  "available_models": [
    {
      "name": "qwen2_5-7b",
      "description": "Qwen2.5 7B instance",
      "type": "text",
      "tool_calling": "native",
      "max_prompt_size": 2047,
      "enabled": true
    }
  ]
}

 

Sending a Test Request


Once the server is running, a basic request can be sent to the chat completions endpoint:

curl -H 'Content-Type: application/json' \
  -d '{
    "model": "Qwen2.5-7B-Instruct",
    "messages": [
      {
        "role": "user",
        "content": "Who are you?"
      }
    ]
  }' \
  -X POST 0.0.0.0:8000/v1/chat/completions

The API can also be tested from the OpenAPI UI at:

http://0.0.0.0:8000/docs

 

Walkthrough Video


In the attached video, I show how to start the eIQ AAF Connector, verify the server is running, configure a model, and send a sample request to the /v1/chat/completions endpoint.

(view in My Videos)

 

Summary


The eIQ AAF Connector provides the REST API layer for running edge AI models on NXP i.MX platforms with Ara240 DNPU acceleration. It allows applications to send prompts, receive generated responses, and integrate local LLM or VLM inference into demos, prototypes, and edge AI workflows.

 

Link

 

ARA2-M2-16G-GTARA240Hands-On Training
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-02-2026 08:07 AM
更新者: