2371436_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2371436_en-US

2371436_en-US

FreeRTOS 2.0.0 is not available

I am setting up MR-CANHUBK344s with the S32 design example project. I have found the downloads for S32K3 RTD AUTOSAR 4.4 version 2.0.0 and S32K3xx development package Version 3.4.3, but the FreeRTOS for S32K3 2.0.0 is no longer available for download. The closest I find is 2.0.1 which does not work. 

The file needed is SW32K3_FreeRTOS_10.4.6_2.0.0_D2204.zip 

Can someone share the link to this version?

Re: FreeRTOS 2.0.0 is not available

Hi 

You cannot see the product because it is archived. It means there can be bugs in it, that will not be fixed. We usually recommend that customers use the newer version.

However, if you insist on testing the older version, then please wait while I contact the internal team to inquire how to add the software to your account.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

标记 (1)
无评分
版本历史
最后更新:
‎05-30-2026 04:02 AM
更新人: