2371104_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2371104_en-US

2371104_en-US

MMOexp:Warborne: Above Ashes Void Weapons Guide

In the brutal battlefield of Warborne: Above Ashes, few weapon archetypes are as terrifying or strategically oppressive as the Void Weapons. While other classes rely on raw burst damage, mobility, or defensive utility, Void users specialize in one thing above all else: overwhelming enemies through relentless attrition. Their toolkit revolves around Plague, a devastating status effect that weakens opponents, Warborne Above Ashes Solarbite, and turns prolonged fights into nightmares.

Void Weapons are not simply about dealing damage. They dominate engagements by corrupting enemy positioning, limiting mobility, draining survivability, and creating constant pressure that forces opponents into mistakes. Whether you are fighting in PvP skirmishes, large-scale guild wars, or difficult PvE encounters, understanding how Void abilities synergize together is essential for maximizing their potential.

This article breaks down every major Void Weapon ability, explores the importance of the Plague mechanic, and explains why Void builds are rapidly becoming one of the most feared archetypes in Warborne: Above Ashes.

The Core Identity of Void Weapons

At the center of every Void build is the Plague debuff. Nearly every skill in the Void arsenal either applies Plague directly or amplifies its effects through crowd control and debuffs. Unlike simple damage-over-time mechanics found in many MMOs, Plague acts as a layered pressure system. The longer enemies remain exposed, the weaker and more vulnerable they become.

This creates a combat style focused on sustained dominance rather than immediate elimination. Void players excel in prolonged engagements where they can slowly choke enemy resources, reduce healing efficiency, and control movement.

The strength of Void Weapons comes from three major factors:

Continuous area denial

Multi-target pressure

Stacking debuffs that cripple enemy performance

Because of this, Void users are especially effective in coordinated team fights where allies can capitalize on weakened enemies.

Touch of Plague – The Foundation of Every Void Build

Every Void Weapon begins with the passive attack ability known as Touch of Plague. On the surface, it appears simple: basic attacks deal 90% Magic Damage and apply Plague. However, this ability forms the backbone of the entire archetype.

Unlike weapons that rely heavily on cooldown bursts, Void users constantly apply pressure through ordinary attacks. Every strike contributes to long-term damage scaling while setting up stronger abilities later in the rotation.

The importance of Touch of Plague becomes especially clear during extended engagements. Opponents cannot simply ignore basic attacks because every hit strengthens the overall Plague presence on the battlefield. Over time, even heavily armored enemies begin to crumble under sustained corruption.

This passive also makes Void Weapons exceptionally strong in group combat. When multiple enemies are infected simultaneously, the battlefield becomes increasingly difficult for healers and frontline tanks to stabilize.

Plague Strike – Reliable Mid-Range Pressure

Plague Strike introduces one of the most versatile tools in the Void arsenal. The skill releases a shockwave in a target direction, dealing 120% Magic Damage while inflicting Plague on every enemy hit.

This ability excels because of its straightforward reliability. The linear projectile allows Void players to pressure clustered enemies, punish retreating targets, and safely apply Plague from mid-range distances.

In PvP, Plague Strike becomes particularly dangerous during chokepoint battles. Enemy teams attempting to advance through narrow paths can quickly become infected all at once, creating opportunities for allied damage dealers to follow up.

The ability also works extremely well as an opener. Applying Plague to multiple enemies before activating heavier debuff abilities dramatically increases overall battlefield control.

Because of its speed and reach, Plague Strike is one of the most commonly used abilities in aggressive Void rotations.

Venom Pool – Area Control at Its Finest

One of the defining strengths of Void Weapons is their ability to dictate enemy movement, and Venom Pool perfectly embodies that identity.

This skill throws a venomous pool onto the battlefield that lasts four seconds. Enemies inside are slowed by 20% while receiving Plague every second.

Although the raw damage may seem modest compared to burst-oriented skills, Venom Pool creates immense tactical value. Players trapped within the area become increasingly vulnerable while struggling to reposition effectively.

In large-scale warfare, Venom Pool can completely reshape engagements. Placing it on objectives, choke points, or escape routes forces opponents to either endure constant Plague application or abandon critical positioning.

The skill becomes even more oppressive when combined with allied crowd control. Tanks and melee fighters can pin enemies inside the pool while Void users continuously stack pressure.

Venom Pool is also highly effective defensively. Retreating players can drop the ability behind them to slow pursuers and create breathing room during chaotic fights.

Scourge – Sustained Pressure and Self-Sustain

Scourge is one of the most intimidating single-target abilities available to Void users. The skill channels continuous damage every 0.7 seconds, inflicting Plague while simultaneously restoring 25% HP to the caster.

The tradeoff is mobility. Players cannot move while channeling Scourge, meaning positioning becomes absolutely critical.

When used correctly, however, Scourge can completely swing duels and frontline encounters. The combination of repeated damage ticks and self-healing allows Void players to outlast opponents who rely on burst windows.

This ability is especially devastating against isolated targets. Enemies caught without mobility cooldowns or interrupts can rapidly lose health while the Void user sustains themselves through incoming damage.

Scourge also synergizes exceptionally well with slowing effects from Venom Pool or Plague Surge. Once opponents are immobilized or heavily slowed, escaping the channel becomes significantly more difficult.

In PvE, Scourge serves as a reliable sustain tool during boss encounters and elite farming, allowing Void players to maintain pressure without depending entirely on healers.

Plague Surge – Massive Crowd Pressure

Among all Void abilities, Plague Surge stands out as one of the strongest team-fight initiators.

The ability releases a surge of plague energy in a target direction, dealing 160% Magic Damage, applying two stacks of Plague, and reducing enemy Speed by 30% for four seconds.

This combination is incredibly dangerous because it simultaneously delivers damage, debuffs, and crowd control in a single action.

The double-stack Plague application accelerates the corruption process immediately, making enemies vulnerable much faster than standard attacks alone. Meanwhile, the movement reduction severely limits repositioning options.

Plague Surge is particularly effective when engaging grouped enemies. Landing the ability on multiple targets can instantly shift momentum in favor of your team.

In coordinated PvP scenarios, Void players often use Plague Surge as the opening strike before allies unleash heavy AoE abilities. Slowed enemies become easier targets for follow-up crowd control, ranged attacks, and burst combos.

Because of its high impact and strong scaling potential, Plague Surge is often considered a mandatory skill in competitive Void builds.

Spread Plague – Constant Battlefield Oppression

If there is one skill that truly defines the oppressive identity of Void Weapons, it is Spread Plague.

While active, the ability continuously consumes MP every three seconds and automatically inflicts Plague on nearby enemies. Opponents also suffer a 30% chance for basic attacks to miss for five seconds.

This ability transforms Void users into walking zones of corruption.

In prolonged fights, Spread Plague creates enormous passive pressure simply by existing near enemy players. Melee fighters struggle to maintain efficiency because missed attacks dramatically reduce damage consistency.

The psychological effect is equally powerful. Opponents are forced to either disengage entirely or remain inside an increasingly punishing aura.

Spread Plague shines brightest during large-scale warfare and objective control. Void players can push directly into enemy formations and destabilize entire frontlines through passive debuffs alone.

However, the ability requires careful MP management. Poor resource control can leave players vulnerable after exhausting mana reserves. Skilled Void users know exactly when to activate or deactivate Spread Plague depending on the pace of battle.

Exhaustion – One of the Strongest Debuff Skills in the Game

Exhaustion may be the single most strategically powerful utility skill available to Void Weapons.

The ability creates a draining field lasting six seconds. Enemies inside are slowed by 30% while receiving stacks of Exhaustion every second. Each stack reduces Damage Boost, Healing Bonus, and Attack Speed by 6%, stacking up to six times.

At maximum stacks, enemies suffer catastrophic stat reductions:

36% reduced Damage Boost

36% reduced Healing Bonus

36% reduced Attack Speed

This is absolutely devastating in organized PvP.

Healers become dramatically less effective. DPS players lose offensive momentum. Tanks struggle to maintain threat and sustain. Entire enemy formations can collapse if trapped inside the field too long.

Exhaustion works especially well during sieges and defensive holds. Placing the field around objectives forces enemies to either retreat or fight while severely weakened.

Combined with Venom Pool and Spread Plague, Exhaustion creates layered zones of denial that can completely dominate terrain control.

Many experienced players already consider Exhaustion one of the strongest utility abilities currently available in Warborne: Above Ashes.

Toxic Matter – Chain Corruption and Resistance Shredding

Toxic Matter represents the high-skill, high-value side of the Void arsenal.

After a brief cast time, the projectile launches toward a target and bounces between enemies up to nine times. Each hit deals 120% Magic Damage, applies Plague, and reduces Magic Resistance by 15% for four seconds.

This ability becomes incredibly dangerous in clustered fights.

The bouncing mechanic allows Toxic Matter to spread corruption rapidly through entire enemy groups while simultaneously amplifying magical damage from allied casters.

The Magic Resistance reduction is particularly important because it strengthens not only the Void player’s own abilities but also the effectiveness of allied magic users.

In coordinated guild battles, Toxic Matter often serves as the setup tool for devastating magical burst combinations.

The bounce limit also rewards intelligent targeting. Skilled players aim at central enemies to maximize spread efficiency and ensure the debuff reaches priority targets.

Because each enemy can only be hit twice, positioning and timing become critical factors in mastering the skill.

Why Void Weapons Are Becoming Meta

The growing popularity of Void Weapons in Warborne: Above Ashes comes down to versatility.

Few archetypes can simultaneously:

Control space

Apply sustained AoE pressure

Reduce enemy effectiveness

Support allied damage

Maintain self-sustain

Dominate prolonged engagements

Void users thrive in nearly every type of combat scenario. Small-scale duels reward their sustain and attrition. Large-scale wars amplify their debuff potential. PvE encounters benefit from their constant pressure and survivability.

Most importantly, Void Weapons punish mistakes harder the longer fights continue. Enemies who fail to disengage early often find themselves trapped in overlapping debuffs with little chance of recovery.

As the competitive meta evolves, Void players are quickly becoming essential members of organized groups and guild compositions.

Final Thoughts

Void Weapons in Warborne: Above Ashes are more than simple damage dealers. They are battlefield corrupters designed to dismantle enemy formations piece by piece through relentless pressure and debilitating effects.

From the constant infection of Touch of Plague to the overwhelming debuffs of Exhaustion and the chain devastation of Toxic Matter, every skill contributes to a combat style built around domination through attrition cheap Warborne Above Ashes Solarbite.

Players who enjoy strategic warfare, area denial, and methodical battlefield control will likely find Void Weapons among the most rewarding archetypes in the game. While they may lack the flashy burst of assassin classes or the straightforward durability of tanks, their ability to weaken entire enemy teams makes them one of the most dangerous forces currently emerging in Warborne: Above Ashes.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎05-30-2026 04:46 AM
更新者: