Hello,
I am try to download S32K344 example image s32k3_wb_can.elf to EVB, but it fail and prompt is "Error while launching command arm-none-eabi-gdb --version".
I can compile the s32k3_wb_can project normally. The debugger is GDB SEGGER J-link, and it can burning another HEX file to EVB via Jflash SW tools. So, the EVB and H/W have no problem.
The installed SW in S32DS is as follows.
The arm-none-eabi-gdb.exe also exist in my S32DS install folder D:\NXP\S32DS.3.4 and it can run in windows env.
The debug Configuration setting is as follows:
I can't find the problem. Could you please help find where is the problem? Thanks.
Hi
Please refer to the configuration mentioned in S32 Design Studio for S32 Platform V3.4/V3.5 + SEGGER J-LINK Plus
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.