As the title suggests, I need some help or maybe a push in the right direction I should say.
NXP provides these types of SDKs (LSDK, LLDP). I’m real confused what I’m supposed to use. LLDP provides these types of massive Linux Distro solutions. I don’t need this, I need an embedded solution.
With Xilinx chips it’s simple, the answer is petalinux. However, NXP’s LLDP has all these options for building out these crazy heavy duty Linux builds. I need some help in understanding how/what NXP SDK to use to create an embedded solution.
If you have a bit of experience with this would you be so kind to provide me some direction please?
LLDP provides Ubuntu Linux.
For Debian Linux, you could refer to the following link.
If you want to use the latest simple yocto project, you could refer to the following link.