Hello,
Getting a failed stage 2 status each time after we do a hsm download. This status remains as failed even after a successful application download.
Fbl_Port_BM_SpResponse after Fbl_Port_BM_InitializeInterface:
x03 (0x03),
x01 (0x01),('Q' (0x51),
x00 (0x00)),
x01 (0x01))
Any insights into this?
Best regards.
This is OEM specific security firmware which is not supported by our team on this public community.
Please create a ticket here and it will be assigned to responsible regional FAE team:
https://support.nxp.com/s/?language=en_US
Regards,
Lukas
Using NXP S32 K388
MCAL+ LLSI : SW32K3_RTD_R21-11_7.0.1_P05_D2604 + LLSI_SW32K3XX_0_9_10_PRC
hse : hse_fw_s32k388_12_2_108_0
We observe that hsm will always return a failed Stage 2 status after we execute a successful hsm download routine.
This happens with secure boot ON.
Before the download, there are no reported stage failures.
You haven’t provided enough information to properly investigate the issue. Please include more context and a detailed problem description, specify the exact MCU you are using, and indicate which software/firmware or tools are involved.
Regards,
Lukas